I am getting an error when CCS asks to update the firmware on a BRAND NEW out of the box MSP-FET:
MSP430: Error: MSP-FET / eZ-FET recovery failed
Digging around, I find a batch file in
C:\ti\ccsv6\ccs_base\DebugServer\drivers
So I run v2v3.bat and it complains:
******************************************************************
WARNING
Do NOT run this updater with more than one emulator connected.
Multiple connected MSP-FET430UIF or eZ430 emulators may cause the upgrade
to fail and render the emulator unusable.
Please ensure to disconnect all emulators except for the intended MSP-FET430UIF.
******************************************************************
Enter 'y' to confirm: y
Initialize: done
MSP430_FET_GetFwVersion()
Could not read Firmware version, exiting
Press any key to close this application.
Press any key to continue . . .
Looking in Device Manager, I see no devices named 'MSP-FET'. When I plug/unplug the MSP-FET, I see Windows add a 'USB Input Device'.
So I am wondering if there are no drivers for W10 yet, and it is installing the MSP-FET as a USB input device???
Need some help here, somebody toss me a clue? I have deleted/reinstalled CCS three times now, no joy.