Other Parts Discussed in Thread: TM4C1294NCPDT
Hi,
I'm currently working on a design using an MSP432P401R, and am interested in implementing a version of the XDS110-ET onboard. I think I have a reasonable grasp on the hardware design and can manage it based on the available schematics from the launchpad, but I am having trouble tracking down the software for the programmer.
A while back I stumbled upon the firmware for the EZ-FET programmers on the MSP430 line for a similar project, but can't seem to track it down again.
I would appreciate it if anyone could point me in the proper direction of the firmware for the XDS110 programmer, as well as let me know if there are any major roadblocks I should foresee.
I know the EZ-FET lite devices had another MSP430 as their core that had a USB BSL that was used to set up the programmer initially, at least to my understanding. Then it simply acted as a source for spy bi wire debugging, along with a USB hub to implement the backchannel UART and such. The processor used in the XDS110-ET schematics isn't an MSP, so it doesn't have a BSL in that sense. I'm assuming it will have to be initially configured by a standard JTAG programmer?
Thanks for all your help!
- Jesse