Other Parts Discussed in Thread: MSP430G2553, MSP430F5438A, ENERGIA
I have been searching on how to interface MSP430G2553 with ADXL345 using I2C. I found example code in many forums, but all of them are incomplete or buggy. I finally managed to modify the example code from this post and made it work! I also added a functionality to print the x,y,z values out to serial port through UART.
I saw many people replied in those forums saying that they couldn't get them working, so I decided that I should share my working solution here.
Hardware Setup
First, make sure the connection between MSP430 and ACXL346 is correct.
This diagram is modified from this site.
Program
The program below read x,y,z accelerometer values every one second and print the values out to the serial port using UART. It also turns on or off the red LED according to the x and y values. Don't worry if you don't have UART set up properly, the code should still works. If you want to enable UART, don't forget to rotate the RXD and TXD jumpers on J3 by 90 degrees on the lauchpad. The UART interfacing code is modified from this site.
Here is my complete program.
// Interfacing ADXL345 accelerometer with MSP430G2553 with I2C communication // and printing restuls to serial port using UART. // // /|\ /|\ // ADXL345 10k 10k MSP430G2xx3 // slave | | master // ----------------- | | ----------------- // | SDA|<-|---+->|P1.7/UCB0SDA XIN|- // | | | | | // | | | | XOUT|- // | SCL|<-+----->|P1.6/UCB0SCL | // | | | | // // For Sparkfun ADXL345, // * connect SDO to ground // * connect CS to VCC // // Original I2C code by : // Prof. Ravi Butani // Marwadi Education Foundation, Rajkot GUJARAT-INDIA // ravi.butani@marwadieducation.edu.in // e2e.ti.com/.../260094 // // Original UART code by : // Benn Thomsen // bennthomsen.wordpress.com/.../ // // // Modified By : // Phitchaya Mangpo Phothilimthana // mangpo@eecs.berkeley.edu //****************************************************************************** #include <msp430g2553.h> #define NUM_BYTES_TX 2 #define NUM_BYTES_RX 6 #define ADXL_345 0x53 int RXByteCtr; volatile unsigned char RxBuffer[6]; // Allocate 6 byte of RAM unsigned char *PRxData; // Pointer to RX data unsigned char TXByteCtr, RX = 0; unsigned char MSData[2]; // Functions for I2C void Setup_TX(unsigned char); void Setup_RX(unsigned char); void Transmit(unsigned char,unsigned char); void TransmitOne(unsigned char); void Receive(void); // Function for UART: printing output to serial port void Setup_UART(); void UARTSendArray(unsigned char *TxArray, unsigned char ArrayLength); void UARTSendInt(unsigned int x); int main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop WDT // LED P1DIR |= BIT0; // P1.0 = red LED P1OUT |= BIT0; // P1.0 = red LED // UART BCSCTL1 = CALBC1_1MHZ; // Set DCO to 1MHz DCOCTL = CALDCO_1MHZ; // Set DCO to 1MHz // Configure hardware UART P1SEL |= BIT1 + BIT2 ; // P1.1 = RXD, P1.2=TXD P1SEL2 |= BIT1 + BIT2 ; // P1.1 = RXD, P1.2=TXD // ADXL345 P1SEL |= BIT6 + BIT7; // Assign I2C pins to USCI_B0, P1.6 = SCL, P1.7 = SDA P1SEL2 |= BIT6 + BIT7; // Assign I2C pins to USCI_B0, P1.6 = SCL, P1.7 = SDA // Init sequence for ADXL345 Setup_TX(ADXL_345); Transmit(0x2D,0x00); while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent Setup_TX(ADXL_345); Transmit(0x2D,0x10); while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent Setup_TX(ADXL_345); Transmit(0x2D,0x08); while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent // Un-comment next block to change range of ADXL345 /* Setup_TX(ADXL_345); RPT_Flag = 1; Transmit(0x31,0x01); // Range Select at add 0x31 write 0x00 for 2g(default)/ 0x01 for 4g/ 0x02 for 8g/ 0x03 for 16g while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent */ while(1){ // Transmit process Setup_TX(ADXL_345); TransmitOne(0x32); // Request Data from ADXL345 in 2g Range 10Bit resolution while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent // Receive process Setup_RX(ADXL_345); Receive(); while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent int x = (((int)RxBuffer[1]) << 8) | RxBuffer[0]; int y = (((int)RxBuffer[3]) << 8) | RxBuffer[2]; int z = (((int)RxBuffer[5]) << 8) | RxBuffer[4]; // Now we have x,y,z reading. // Below red LED is on, if x or y angle is more then 45 or less then -45 degree. if ((x > 128) || (y > 128) || (x < -128) || (y < -128)) { P1OUT |= BIT0; // red LED on } else { P1OUT &= ~BIT0; // red LED off } // Print x,y,z to serial port in hew. Setup_UART(); UARTSendArray("sample\n", 7); UARTSendInt(x); UARTSendInt(y); UARTSendInt(z); __delay_cycles(1000000); // delay 1 sec } } //------------------------------------------------------------------------------- // I2C //------------------------------------------------------------------------------- #pragma vector = USCIAB0TX_VECTOR __interrupt void USCIAB0TX_ISR(void) { if(RX == 1){ // Master Recieve? RXByteCtr--; // Decrement RX byte counter if (RXByteCtr) { *PRxData++ = UCB0RXBUF; // Move RX data to address PRxData } else { UCB0CTL1 |= UCTXSTP; // No Repeated Start: stop condition *PRxData++ = UCB0RXBUF; // Move final RX data to PRxData __bic_SR_register_on_exit(CPUOFF); // Exit LPM0 }} else{ // Master Transmit if (TXByteCtr) // Check TX byte counter { TXByteCtr--; // Decrement TX byte counter UCB0TXBUF = MSData[TXByteCtr]; // Load TX buffer } else { UCB0CTL1 |= UCTXSTP; // I2C stop condition IFG2 &= ~UCB0TXIFG; // Clear USCI_B0 TX int flag __bic_SR_register_on_exit(CPUOFF); // Exit LPM0 } } } void Setup_TX(unsigned char Dev_ID){ _DINT(); RX = 0; IE2 &= ~UCA0RXIE; // Disable USCI_A0 RX interrupt (UART) IE2 &= ~UCB0RXIE; // Disable USCI_B0 RX interrupt (I2C) while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent// Disable RX interrupt UCB0CTL1 |= UCSWRST; // Enable SW reset UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset UCB0BR0 = 12; // fSCL = SMCLK/12 = ~100kHz UCB0BR1 = 0; UCB0I2CSA = Dev_ID; // Slave Address is 048h UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation IE2 |= UCB0TXIE; // Enable TX interrupt } void Setup_RX(unsigned char Dev_ID){ _DINT(); RX = 1; IE2 &= ~UCA0RXIE; // Disable USCI_A0 RX interrupt (UART) IE2 &= ~UCB0TXIE; // Disable USCI_B0 TX interrupt (I2C) UCB0CTL1 |= UCSWRST; // Enable SW reset UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset UCB0BR0 = 12; // fSCL = SMCLK/12 = ~100kHz UCB0BR1 = 0; UCB0I2CSA = Dev_ID; // Slave Address is 048h UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation IE2 |= UCB0RXIE; // Enable RX interrupt } void Transmit(unsigned char Reg_ADD,unsigned char Reg_DAT){ MSData[1]= Reg_ADD; MSData[0]= Reg_DAT; TXByteCtr = NUM_BYTES_TX; // Load TX byte counter while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition __bis_SR_register(CPUOFF + GIE); // Enter LPM0 w/ interrupts } void TransmitOne(unsigned char Reg_ADD){ MSData[0]= Reg_ADD; TXByteCtr = 1; // Load TX byte counter while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition __bis_SR_register(CPUOFF + GIE); // Enter LPM0 w/ interrupts } void Receive(void){ PRxData = (unsigned char *)RxBuffer; // Start of RX buffer RXByteCtr = NUM_BYTES_RX; // Load RX byte counter while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent UCB0CTL1 |= UCTXSTT; // I2C start condition __bis_SR_register(CPUOFF + GIE); // Enter LPM0 w/ interrupts } //------------------------------------------------------------------------------- // UART //------------------------------------------------------------------------------- void Setup_UART() { _DINT(); IE2 &= ~UCB0RXIE; // Disable USCI_B0 RX interrupt (I2C) IE2 &= ~UCB0TXIE; // Disable USCI_B0 TX interrupt (I2C) UCA0CTL1 |= UCSSEL_2; // Use SMCLK UCA0BR0 = 104; // Set baud rate to 9600 with 1MHz clock (Data Sheet 15.3.13) UCA0BR1 = 0; // Set baud rate to 9600 with 1MHz clock UCA0MCTL = UCBRS0; // Modulation UCBRSx = 1 UCA0CTL1 &= ~UCSWRST; // Initialize USCI state machine IE2 |= UCA0RXIE; // Enable USCI_A0 RX interrupt } // Print an array of char void UARTSendArray(unsigned char *TxArray, unsigned char ArrayLength){ while(ArrayLength--){ // Loop until StringLength == 0 and post decrement while(!(IFG2 & UCA0TXIFG)); // Wait for TX buffer to be ready for new data UCA0TXBUF = *TxArray; // Write the character at the location specified py the pointer TxArray++; //Increment the TxString pointer to point to the next character } IFG2 &= ~UCA0TXIFG; // Clear USCI_A0 int flag } // Print int in hex void UARTSendInt(unsigned int x){ unsigned char buff[10]; unsigned char data[10]; unsigned char index = 0, i = 0; while(x > 0) { unsigned char val = x % 16; if(val < 10) buff[index] = 48+val; else buff[index] = 97+val-10; index++; x /= 16; } buff[index] = '\n'; while(index > 0) { index--; data[i] = buff[index]; i++; } if(i==0) { data[0] = '0'; i++; } data[i] = '\n'; UARTSendArray(data, i+1); }