Other Parts Discussed in Thread: TPS735
Hi!
I bought myself a nice TFT Display lately and am working on controlling it with the MSP432 launchpad. But before running it, I have a question regarding the power the lauchpad can supply. The datasheet of the Display states that the maximum current consumption of the panel including the backlight is 450 mA (at 3,3V). I've read that the USB 3.0 port, on which the launchpad is (without a hub) directly connected can provide up to 900 mA. In the datasheet of the launchpad is no maximum current defined, but this Thread states that the XDS110-ET can provide up to 500 mA. This figure
of the launchpad datasheet states that the left header is directly connected to the power supply of the XDS110-ET, hence could provide the required 450 mA. I know, this is just a sketch of the schematic, but I couldnt find any other information regarding this. Would you say I can connect the Display to that header safely or are there any power related issues to consider? I would run it with only half the brightness max possible to make sure all the other peripherals and the CPU get enough current.
Alternatively, there is a 3.3V supply on the XDS110-ET side of the launchpad. I have not measured it yet but is supplying the display from that pin a better option?
Thanks for you answers in advance
Jonathan