This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 writing IR in NEC format



Hi,

What is the easiest way to write NEC remote data to an IR LED at 38kHz?

For example i now the code for power on on my device i.e 0x111E30CF,  unsigned int data = 0x111E30CF

is there sample code for transmission?

thanks

  • Hello!

    Unfortunately there is no miracle method because there is no IR engine in MSP430.
    There is an IRDA, but this is different.

    Note that Google is your friend:
    www.circuitvalley.com/.../nec-protocol-ir-infrared-remote-control.html

    Now for the particular implementation on MSP430, what I do is as follows:
    - Configure a timer based on SMCLK to generate a square 38 KHz wave (can be easily
      started and stopped using OUTMOD).
    - Configure another timer based on ACLK to generate your bit encodings.
      Usually, on all the remote controls I have experienced, a 0 is made of 2 equal
      periods: 1 period with pulses and one period with no pulses. And a 1 is made of
      2 periods, one being generally double of the second one.

    The good thing about using pwm timers is that at least you don't need to interrupt
    all the time to generate 38 kHz pulses (in this case, you should interrupt at 76
    kHz, and toggle the putout). What you do is set the 38 kHz wave and clear it.
    Therefore one interrupt every 560 µs at most.
    I haven't found any smarter way to do it.

    Have fun!

    Pascal

  • The MSP430FR413x chips has IR modulation Logic. There are many IR remote control examples for FR4133 LunchPad and Infrared (IR) BoosterPack Plug-in Module

  • Hello!
    Good to know that. Are there other IR capable devices?
    Pascal
  • I did not see any other MSP with the IR modulation Logic. But it is not a big thing; I think you did that in firmware.

**Attention** This is a public forum