Other Parts Discussed in Thread: MSP430F6736, MSP-FET
hi
i have a msp430-fet430uif debugger...ccsv6.1.1.00022 on win7 64bit...as i started the last debug session a few minutes ago i was asked to upgrade the firmware on the fet, which i duly did.
However, after it had upgraded and then carried on to get to the 1st statement in 'main' i got this error...
"MSP430: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x6978: Address is past the end of memory"
How can i fix my problem...i dont know where this finish auto run even comes from nor the address....in fact, what IS the problem?
in addition, i see that where it stopped is at the start of boot_special.c which is a file i've never seen before.
thanks in advance