This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-FET How address two programmer on one PC

Other Parts Discussed in Thread: MSP-FET, MSP-GANG, MSP430-FLASHER

Hello,

we need use two MSP-FET programmer on one PC.  

How use two unit in command line? 

In manual is mention only USB connection without S/N of each unit.

Pavel 

  • Hello Pavel,

    What MSP programming interface are you working with? Each MSP-FET enumerates as a MSP Application UART1 and Debug Interface as shown inside of your PC's device manager. My best guess is that you are using MSP430-FLASHER, in which case you can use the -i trigger to distinguish between multiple MSP-FET Debug Interfaces. The two FET devices cannot work in parallel, you will need to program your units using one FET at a time. If you would like to program multiple devices at the same time then you should consider using a MSP-GANG.

    Regards,
    Ryan

**Attention** This is a public forum