This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1110 with temperature sensor using I2C

hi,


I'm working on a project and i need to connect the CC1110 with MCP9808 (temperature sensor).

The problem is that MCP9808 uses I2C connection and the CC1110 chip has no such interface.

I did a little research and it seems the problem can be solve by using bit banging method but i cant find any really good example or document explaining how to do it. 

So i ask to the TI  community if someone knows how to do it or if there is another method that i can use in order to complete this task. Any help is precious.

Thanks.

**Attention** This is a public forum