My problem is this, I have a MSP432P401R + CC2564MODNEM (linked via EM Adapter BoosterPack) and I want to set my CC2564MODNEM using GNU to use the SPP profile to send a serial BAUDRATE that allows me to send bytes at a speed of 1Mbps.
Performing a search I found a library BLUETOPIA to record MSP432, but I have not managed to set the CC2564.
They know if there are any friendly method of configuring the SPP profile in the CC2564MODNEM or if there is firmware for it?
From now I thank them for the help!
Regards,
Franco La Paz