Hi,
My schematic is as follows.
The "V3.3M" is from a LDO with the output 3.3V. I measure the "nRST" level, and the value isn't pulled up to 3.3V. It's not stable and the MSP432 cannot work correctly.
Any advice will be appreciated.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My schematic is as follows.
The "V3.3M" is from a LDO with the output 3.3V. I measure the "nRST" level, and the value isn't pulled up to 3.3V. It's not stable and the MSP432 cannot work correctly.
Any advice will be appreciated.
>I measure the "nRST" level, and the value isn't pulled up to 3.3V.
Sayting that it is not 3.3V does not help much. What did you measure? exactly 3.2999V or 0? There are no any reports about reset problem you mention so you shall check against simple PCB soldering or routing error or PCB dirt or deffective capacitor. After alll pin 83 is between pins 82 and 84, both connected to GND
user4484512 said:The level of the RESET pin is a value between 0V and 3.3V, sometimes 1.2V, sometimes 2.4V
But you do not measure this pin while a debug probe like the MSP-FET is connected and active?
**Attention** This is a public forum