This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to debug using CCS in MSP432.

Other Parts Discussed in Thread: ENERGIA

I am unable to debug and burn the code into MSP432 .  It gives me the following error .

CORTEX_M4_0: GEL Output: Memory Map Initialization Complete
CORTEX_M4_0: GEL Output: Halting Watchdog Timer
CORTEX_M4_0: Flash Programmer: Erasing main memory
CORTEX_M4_0: Flash Programmer: Writing 2020 bytes to flash memory 0x00000000
CORTEX_M4_0: JTAG Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.222.0)


I tried MSP432 factory reset and then tried to debug an empty code (below) still getting the same error .

#include "msp.h"

void main(void)
{

WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer

}

When i try in energia it works fine . Please help me in this regard...

**Attention** This is a public forum