This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Not supported by selected Interface or Interface is not initialized

Other Parts Discussed in Thread: MSP430F1612

I'm trying to Download and Debug on my MSP430F1612 for the first time.

It's a very simple program:

#include "msp430.h"                     ; #define controlled include file

        NAME    main                    ; module name

        PUBLIC  main                    ; make the main label vissible
                                        ; outside this module
        ORG     0FFFEh
        DC16    init                    ; set reset vector to 'init' label

        RSEG    CSTACK                  ; pre-declaration of segment
        RSEG    CODE                    ; place program in 'CODE' segment

init:   MOV     #SFE(CSTACK), SP        ; set up stack

main:   NOP                             ; main program
        MOV.W   #WDTPW+WDTHOLD,&WDTCTL  ; Stop watchdog timer
        BIS.B   #1h, P1DIR              ; set P1.1 to output mode
        XOR.B   #1h, P1OUT              ; Toggle Red LED on MSP430F1612
        JMP $                           ; jump to current location '$'
                                        ; (endless loop)
        END


Every time I try and download and debug I get:


Wed Oct 12, 2016 00:12:17: Not supported by selected Interface or Interface is not initialized : (Configure) , mode=0x8, value=0x0
Wed Oct 12, 2016 00:12:17: Not supported by selected Interface or Interface is not initialized : (Configure) , mode=0x8, value=0x0
Wed Oct 12, 2016 00:12:17: Not supported by selected Interface or Interface is not initialized : (Configure) , mode=0x8, value=0x0
Wed Oct 12, 2016 00:12:17: Not supported by selected Interface or Interface is not initialized : (Configure) , mode=0x8, value=0x0
Wed Oct 12, 2016 00:12:17: Not supported by selected Interface or Interface is not initialized : (Configure) , mode=0x8, value=0x0
Wed Oct 12, 2016 00:12:17: Not supported by selected Interface or Interface is not initialized : (Configure) , mode=0x8, value=0x0

Wed Oct 12, 2016 00:12:20: Fatal error: Failed to re-initialize   Session aborted!


This is for school and this is the 1st time I've used the MSP430, CCS, or IAR Embedded Workspace IDE.

I'm at my wits end. I've googled those errors to death and haven't found anything useful. Any help would be appreciated.









**Attention** This is a public forum