Tool/software: Code Composer Studio
Hi,
I am using MSP432P401R launchpad and CCS 6.2.0.00050. Suddenly I am not able to program or debug it. I have even tried the out of the box msp432 example. I am getting the following errors in the Debug Console.
CORTEX_M4_0: * WARNING *: The connected device is not MSP432P401R
CORTEX_M4_0: GEL Output: Memory Map Initialization Complete
CORTEX_M4_0: GEL Output: Halting Watchdog Timer
CORTEX_M4_0: WARNING : On MSP432P401R hitting a breakpoint cannot be detected by the debugger when the device is in low power mode.
Click the pause button during debug to check if the device is held at the breakpoint.
CORTEX_M4_0: Flash Programmer: Reading HW revision failed.
CORTEX_M4_0: Your XMS432P401R material is no longer supported. We recommend you moving to production-quality MSP432P401R/M silicon by ordering samples at www.ti.com/product/MSP432P401R.
CORTEX_M4_0: File Loader: Memory write failed: Unknown error
CORTEX_M4_0: GEL: File: C:\Users\ABHAY\Desktop\ccs_practice\TEST_432\Debug\TEST_432.out: Load failed.
I tried searching in the e2e forums and I think I have bricked my MSP432. Accordingly I tried to Factory Reset the MSP432, but at the end step when I try to run the SCRIPT menu, it shows there aren't any scripts available.
Hoping for help in this regard as soon as possible.
Regards,
Amit Kotal