Tool/software: Code Composer Studio
Hi all,
The problem with the i2c driver is I can't do a write after a single byte read.
I've tested and can read 2, 4, up to 32 bytes after a write, no problem, but if I do a read 1 byte, the next write waits for a transmit interrupt that never occurs.
I can clear the error by doing another write followed by then write then reading more than 1 byte - which sometimes fails and sometimes does not, and sometimes this takes two write-read cycles to clear.
Using bus pirate to write / read the i2c bus or single byte reads is not a problem (i.e. generating independent ground truth), which more or less leads me to conclude it is a problem with the 432 chip or with the driverlib.
Using this forum, I see other people have had the same or similar problems- that appear unresolved, which leads me to conclude that is just might be a real problem and not me.
Any help - in either direction - from you to me or from me to you? I can run tests, I can send you code, whatever...
thx,
bob s.