Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hello fellows,
I made a code to interact the MSP430, with the LCD, but now I would like to have it interact with the MSP432.
And I'm having some problems because I want to use specific pins, can anyone help me change the code?
My difficulty is: the MSP430 I use PORT P1 and P2, the problem is in the MSP432 I need PORT P2, P5 and P6
This is my connections LCD->MSP432:
EN -> (P2 + BIT3)
RS -> (P6 + BIT7)
D4 -> (P2 + BIT6)
D5 -> (P2 + BIT4)
D6 -> (P5 + BIT6)
D7 ->(P6 + BIT6)
/*****************************************************************/
/********* INCLUDE *********/
/*****************************************************************/
#include "lcd.h"
/*****************************************************************/
/********* DEFINES *********/
/*****************************************************************/
#define P1orP2lcd 0x0200
#define EN (PP2 + BIT5)
#define RS (PP1 + BIT3)
#define D0 (PP2 + BIT1)
#define D1 (PP2 + BIT2)
#define D2 (PP2 + BIT3)
#define D3 (PP2 + BIT4)
//#define BACKLIGHT (PP1 + BIT0)
// Commands
#define CLEAR 0x01
/*****************************************************************/
/********* LOCAL FUNCTIONS *********/
/*****************************************************************/
void lcdDirPinout(unsigned int pin)
{
if(pin < P1orP2lcd){
P1DIR |= (pin & 0x00FF);
}else{
P2DIR |= (pin & 0x00FF);
}
}
/*
*
*/
void lcdSetPinout(unsigned int pin)
{
if(pin < P1orP2lcd){
P1OUT |= (pin & 0x00FF);
}else{
P2OUT |= (pin & 0x00FF);
}
}
void lcdClrPinout(unsigned int pin)
{
if(pin < P1orP2lcd){
P1OUT &= ~(pin & 0x00FF);
}else{
P2OUT &= ~(pin & 0x00FF);
}
}
void lcdSetValue(unsigned char value)
{
if(value & 0x08){
lcdSetPinout(D3);
}else{
lcdClrPinout(D3);
}
if(value & 0x04){
lcdSetPinout(D2);
}else{
lcdClrPinout(D2);
}
if(value & 0x02){
lcdSetPinout(D1);
}else{
lcdClrPinout(D1);
}
if(value & 0x01){
lcdSetPinout(D0);
}else{
lcdClrPinout(D0);
}
delay_us(5);
}
void lcdTriggerEN()
{
lcdSetPinout(EN);
delay_us(5);
lcdClrPinout(EN);
// delay_us(5);
}
void lcdWriteData(unsigned char data)
{
lcdSetPinout(RS); // Set RS to Data
lcdSetValue(data >> 4); // Upper nibble
lcdTriggerEN();
lcdSetValue(data); // Lower nibble
lcdTriggerEN();
delay_us(30); // Delay > 50 us
}
void lcdWriteCmd(unsigned char cmd)
{
lcdClrPinout(RS); // Set RS to Cmd
lcdSetValue(cmd >> 4); // Upper nibble
lcdTriggerEN();
lcdSetValue(cmd); // Lower nibble
lcdTriggerEN();
delay_ms(2); // Delay > 5ms
}
/*****************************************************************/
/********* GLOBAL FUNCTIONS *********/
/*****************************************************************/
/*
*
*/
void LCD_PortConfig(void)
{
// Direction
lcdDirPinout(D0);
lcdDirPinout(D1);
lcdDirPinout(D2);
lcdDirPinout(D3);
lcdDirPinout(EN);
lcdDirPinout(RS);
}
/*
*
*/
void LCD_Initialize(void)
{
delay_us(80);
P2OUT = 0x03; // Start LCD (send 0x03)
lcdTriggerEN(); // Send 0x03 3 times at 5ms then 100 us
delay_ms(2);
lcdTriggerEN();
delay_ms(2);
lcdTriggerEN();
delay_ms(2);
P2OUT = 0x02; // Switch to 4-bit mode
lcdTriggerEN();
delay_ms(2);
lcdWriteCmd(0x28); // 4-bit, 2 line, 5x8
lcdWriteCmd(0x08); // Instruction Flow
lcdWriteCmd(0x01); // Clear LCD
lcdWriteCmd(0x06); // Auto-Increment
lcdWriteCmd(0x0C); // Display On, No blink
}
void LCD_SetText(char* text, int x, int y){
unsigned int i;
if (x < 16) {
x |= 0x80; // Set LCD for first line write
switch (y){
case 1:
x |= 0x40; // Set LCD for second line write
break;
case 2:
x |= 0x60; // Set LCD for first line write reverse
break;
case 3:
x |= 0x20; // Set LCD for second line write reverse
break;
}
lcdWriteCmd(x);
}
i = 0;
while (text[i] != '\0') {
lcdWriteData(text[i]);
i++;
}
}
void LCD_SetInt(int val, int x, int y)
{
char number_string[16];
sprintf(number_string, "%d", val); // Convert the integer to character string
LCD_SetText(number_string, x, y);
}
void LCD_Clear()
{
lcdWriteCmd(CLEAR);
}
void LCD_LoadSymbols(void)
{
int j;
static char empty[] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
static char heart[] = {0x00, 0x0A, 0x1F, 0x1F, 0x1F, 0x0E, 0x04, 0x00};
static char bat_100[] = {0x0E, 0x1F, 0x1F, 0x1F, 0x1F, 0x1F, 0x1F, 0x1F};
static char bat_75[] = {0x0E, 0x1F, 0x11, 0x1F, 0x1F, 0x1F, 0x1F, 0x1F};
static char bat_50[] = {0x0E, 0x1F, 0x11, 0x11, 0x11, 0x1F, 0x1F, 0x1F};
static char bat_25[] = {0x0E, 0x1F, 0x11, 0x11, 0x11, 0x11, 0x1F, 0x1F};
static char bat_0[] = {0x0E, 0x1F, 0x11, 0x11, 0x11, 0x11, 0x11, 0x1F};
lcdWriteCmd(0x40);
for(j=0;j!=8;j++){
lcdWriteData(empty[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(heart[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_100[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_75[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_50[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_25[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_0[j]);
}
lcdWriteCmd(CMD_END);
}
void LCD_SetSymbol(unsigned char symbol, unsigned char offset, unsigned char line)
{
lcdWriteCmd(line+offset);
lcdWriteData(symbol);
}
/*****************************************************************/
/********* END *********/
/*****************************************************************/
/*****************************************************************/
/*****************************************************************/
/********* INCLUDE *********/
/*****************************************************************/
#include <msp430.h>
#include "main.h"
#include "lcd.h"
/*****************************************************************/
/********* MAIN *********/
/*****************************************************************/
/* START MESSAGE ON LCD */
void APP_Initialize(void){
int i = 0;
LCD_SetText("ECG HOLTER",3 ,0);
LCD_SetText("START",4 ,1);
LCD_SetSymbol(SYMB_HEART,0,ROW_ONE);
for(i=9; i>=0; i--){
LCD_SetInt(i,11,1);
delay_ms(1000);
}
LCD_Clear();
LCD_SetText("PRESS SETUP",3,0);
LCD_SetSymbol(SYMB_BAT100,0,ROW_ONE);
}
/*
* MAIN
*/
int main(void){
WatchDogHold();
LCD_PortConfig();
LCD_Initialize();
APP_Initialize();
while(1){
}
}
/*****************************************************************/
/********* GLOBAL FUNCTIONS *********/
/*****************************************************************/
void WatchDogHold(void){
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
}