This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430f5529 adc12



P6SEL |= BIT0 + BIT1;
ADC12CTL0 = ADC12ON+ADC12MSC+ADC12SHT0_8+ADC12REF2_5V+ADC12REFON; // Turn on ADC12, extend sampling time
                                            // to avoid overflow of results + V ref = 2.5V
ADC12CTL1 = ADC12SHP+ADC12CONSEQ_3;       // Use sampling timer, repeated sequence
ADC12MCTL0 = ADC12INCH_0;                 // ref+=AVcc = 2.5V, channel = A0
ADC12MCTL1 = ADC12INCH_1 + ADC12EOS;
ADC12IE = ADC12IE1; 

I config adc12 for sequence multi channel

but it seem to be not right

I have 2.5 V in my channel but the result in adc < 0x800

Can any body help me

Thank you

**Attention** This is a public forum