Part Number: MSP-FET
Other Parts Discussed in Thread: MSP-TS430PM64F, , MSP430FR5972
Tool/software: Code Composer Studio
From the HW tools user manual (slau278y) I see the following listed as a feature of the MSP-430:
- Software configurable supply voltage between 1.8V and 3.6 V at 100 mA
How do I configure this supply? I am currently reading 1.4V on the VCC on my target board (MSP-TS430PM64F), which is fine for the processor, but I want to power additional circuitry that requires 3.3 V.
I am using CCS Version: 7.0.0.00043 on Windows 7 Enterprise (Service Pack 1)
Regards,