Part Number: MSP-EXP430G2
Other Parts Discussed in Thread: ENERGIA
Hi,
I try to upload example code to MSP Board via Energia but it's not success. Energia shows me about the error message as following details:
Energia: 1.6.10E18 (Windows 10), Board: "MSP-EXP430G2553LP"
<command-line>:0:12: warning: missing whitespace after the macro name [enabled by default]
Sketch uses 760 bytes (4%) of program storage space. Maximum is 16,384 bytes.
Global variables use 20 bytes (3%) of dynamic memory, leaving 492 bytes for local variables. Maximum is 512 bytes.
MSPDebug version 0.22 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2013 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
usbutil: unable to find a device matching 0451:f432
An error occurred while uploading the sketch
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.
I need to know what's wrong and how can I fix it.
thanks