Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
I would like to lock the JTAG/SWD on my MSP432. I am using an MSP-FET-432ADPTR with an MSP-FET to program the chip. I wanted to first make sure I could do a factory reset before I locked the port. Following SLAU575B section 8 to try the factory reset, whenever I right click on the CPU and click show all cores, the DAP doesn't show up to allow me to do a factory reset. I have the target configured for TI MSP430 USB 1.
If I plug into my MSP432 launchpad (and change the target configuration to XDS110) then the DAP shows up and I can do a factory reset.
Is it possible to factory reset using the MSP-FET and adapter board? If not, how else can I perform it on a custom PCB, so that I can safely lock my JTAG?
Thanks a bunch!