Other Parts Discussed in Thread: ENERGYTRACE, MSP430FR5994, MSP430WARE
Tool/software: Code Composer Studio
I recently obtained an MSP-EXP430FR5994 development kit (hardware revision 1.2) and I have been trying the demo examples with EnergyTrace to monitor energy usage. I want to switch to EnergyTrace++ to see what else I can detect, but that option is not available (the "Switch to EnergyTrace++" button on the EnergyTrace menu bar is grayed out). I believe EnergyTrace++ should be available for this hardware and would like to figure out how to enable EnergyTrace++ support.
I am using Code Composer Studio version 7.2.0.00013. Under Windows->Preferences->Code Composer Studio->Advanced Tools->Energy Trace Technology I have the "EnergyTrace+[CPU State]+[Peripheral States]" radio button selected. For my project, under Project->Properties->Debug->MSP43x Options->Low Power Mode Settings I have the "Enable UltraLow Power debug/ LPMx.5 debug" option selected. I can use EnergyTrace, but I can't switch to EnergyTrace++. Is there something else that I need to setup to enable EnergyTrace++?