This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2013: Re-learning how to debug my EZ430 F2013 using IAR Workbench on Windows 10 - Windows 11.

Part Number: MSP430F2013



I know it can be done (even though the docs say it's not supported). I've configured it to work several times in the past. But I don't often use an MSP430 MCU and each time I pick it up again, I have a new computer and the old computer is gone so I have to start from scratch reading documents and forums looking for the secret trick to make this work.

So here goes:

I have an EZ430 (MSP430 F2013 USB thumbdrive device).

- I'm on Windows 11.

- Using IAR Workbench 7.0 (7.10.4)

- Running IAR as ADMINISTRATOR

- I've read the User's Guide steps for opening the sample project and setting the device type appropriately.

- I've read the troubleshooting suggestions and I have gone thru the steps to change the ID of the default TI COM port to COM 2.

- I've followed the instructions to set up a project in IAR from scratch

- Successfully stepping through code execution in Simulator mode. But cannot debug using FET Debugger. (Again, I'm using the sample project for this device.)

RESULT:  

- Best result so far in FET mode is that IAR compiles and links exe but doesn't appear to download. Nothing happens. No LED flashing, no breakpoints hit, nothing.

- There are 2 errors in the Download/Debug process. They look like this:

Invalid parameter(s) : (Configure) , mode=0xe, value=0
Invalid parameter(s) : (RegisterMessageCallback)

Any help greatly appreciated. THANK YOU!

**Attention** This is a public forum