Part Number: MSP430F6779
Hello
About the subject matter of the title.
Although it is about the minimum value of SD24_B, it is "FF00 0000h" manually, but when actually checking, it became "FEFF FFFFh".
The setting is 2's complement oversampling 256.
The maximum value is not a problem.
What other settings are required to make it the numerical value in the manual?
The checked program is a modified MSP 430 F 677 x _ SD 24 B _ 06 so that the result of SD 24 can be displayed on the graph.
<The input wave is a sine wave. In order to check the maximum value and minimum value, it is set to saturation level.>
Regards,
Da