Part Number: MSP430F67791A
Tool/software: Code Composer Studio
Dear All,
I had to configure ADC such that i receive ADC Interrupt every 200uSec on completion of A to D Conversion of all 7 Channels.
I have Configured a timer for 200usec wherein
{
SD24BIE |= SD24BIE6 (Enable interrupt on conversion complete of last channel)
}
I have configured my ADC with below settings for 7 Channels available for SD24B in MSP430F67791A .
{
SD24 Clock : SMCLK = 16MHz
OSR : 256
SD24PDIV = 3
SD24DIV = 0
Left Alignment
Group Conversion
SD24BIE = SD24IE6 (In order to receive interrupt on conversion complete of the Last channel)
}
In ADC Interrupt :
{
Samples are been taken
SD24BIE &= ~SD24IE6 ;
}
The code works absolutely fine i.e. I receive ADC Interrupt every 200uSec, if I the last channel (Channel 6) reading are not been used.(Interrupt enabled for last channel)
Even if i move the Last channel readings (SD24BMEMH6 & SD24BMEML6) into a temp_Variable , the ADC Interrupt in not obtained every 200uSec (it is almost doubled i.e around 400usec).
It is been observed that for what ever channel SD24BIE |= SD24BIE6 ADC Interrupt is been enabled , this behavior repeats i.e. if interrupt enable been done for 5 th channel SD24BIE |= SD24BIE5 ,on handling the results of 5th channel (SD24BMEMH5 & SD24BMEML5) the ADC Interrupt time is altered .
Need your help for solving this issue.
Regards,
Shweta Shelar