Part Number: MSP430F1611
I am currently playing around with TelosB modules, and can get it communciated.
Now, I am trying to print these hexadecimal to decimal as this determines the value of sequence number.
If you look at the code, the number I am really interested is from ASN #1 to # 5 and each ASN is stroed as a byte.
Could someone possibly help me out how to convert 5 bytes of hexadecimal to decimal and print on the screen please?
Thank you
#include "stdint.h"
#include "string.h"
#include "board.h"
#include "radio.h"
#include "leds.h"
#include "uart.h"
#include "sctimer.h"
//=========================== defines =========================================
#define LENGTH_PACKET 125+LENGTH_CRC ///< maximum length is 127 bytes
#define CHANNEL 20
#define LENGTH_SERIAL_FRAME 8 ///< length of the serial frame
//=========================== variables =======================================
typedef struct {
uint8_t num_radioTimerCompare;
uint8_t num_startFrame;
uint8_t num_endFrame;
} app_dbg_t;
app_dbg_t app_dbg;
typedef struct {
// rx packet
volatile uint8_t rxpk_done;
uint8_t rxpk_buf[LENGTH_PACKET];
uint8_t rxpk_len;
uint8_t rxpk_num;
int8_t rxpk_rssi;
uint8_t rxpk_lqi;
bool rxpk_crc;
// uart
uint8_t uart_txFrame[LENGTH_SERIAL_FRAME];
uint8_t uart_lastTxByte;
volatile uint8_t uart_done;
} app_vars_t;
app_vars_t app_vars;
uint8_t count = 25;
//=========================== prototypes ======================================
// radiotimer
//void cb_radioTimerOverflows(void);
// radio
void cb_startFrame(PORT_TIMER_WIDTH timestamp);
void cb_endFrame(PORT_TIMER_WIDTH timestamp);
// uart
void cb_uartTxDone(void);
void cb_uartRxCb(void);
//=========================== main ============================================
/**
\brief The program starts executing here.
*/
int mote_main(void) {
// clear local variables
memset(&app_vars,0,sizeof(app_vars_t));
// initialize board
board_init();
// add callback functions radio
sctimer_setStartFrameCb(cb_startFrame);
sctimer_setEndFrameCb(cb_endFrame);
// setup UART
uart_setCallbacks(cb_uartTxDone,cb_uartRxCb);
// prepare radio
radio_rfOn();
radio_setFrequency(CHANNEL);
// switch in RX
radio_rxEnable();
radio_rxNow();
while (1) {
// sleep while waiting for at least one of the rxpk_done to be set
app_vars.rxpk_done = 0;
while (app_vars.rxpk_done==0) {
board_sleep();
}
// if I get here, I just received a packet
//===== send notification over serial port
// led
leds_error_on();
leds_radio_on();
// format frame to send over serial port
app_vars.uart_txFrame[0] = app_vars.rxpk_buf[0]; // baecon type #1
app_vars.uart_txFrame[1] = app_vars.rxpk_buf[1]; // beacon type
app_vars.uart_txFrame[2] = app_vars.rxpk_buf[17]; // ASN# 1
app_vars.uart_txFrame[3] = app_vars.rxpk_buf[18]; // ASN# 2
app_vars.uart_txFrame[4] = app_vars.rxpk_buf[19]; // ASN# 3
app_vars.uart_txFrame[5] = app_vars.rxpk_buf[20]; // ASN# 4
app_vars.uart_txFrame[6] = app_vars.rxpk_buf[21]; // ASN# 5
app_vars.uart_txFrame[7] = 0xff; // closing flag
app_vars.uart_done = 0;
app_vars.uart_lastTxByte = 0;
// send app_vars.uart_txFrame over UART
uart_clearTxInterrupts();
uart_clearRxInterrupts();
uart_enableInterrupts();
uart_writeByte(app_vars.uart_txFrame[app_vars.uart_lastTxByte]);
while (app_vars.uart_done==0); // busy wait to finish
uart_disableInterrupts();
// led
leds_error_off();
}
}
//=========================== callbacks =======================================
//===== radio
void cb_startFrame(PORT_TIMER_WIDTH timestamp) {
// update debug stats
app_dbg.num_startFrame++;
}
void cb_endFrame(PORT_TIMER_WIDTH timestamp) {
// update debug stats
app_dbg.num_endFrame++;
// indicate I just received a packet
app_vars.rxpk_done = 1;
leds_sync_on();
// get packet from radio
radio_getReceivedFrame(
app_vars.rxpk_buf,
&app_vars.rxpk_len,
sizeof(app_vars.rxpk_buf),
&app_vars.rxpk_rssi,
&app_vars.rxpk_lqi,
&app_vars.rxpk_crc
);
// led
leds_sync_off();
}
//===== uart
void cb_uartTxDone(void) {
uart_clearTxInterrupts();
// prepare to send the next byte
app_vars.uart_lastTxByte++;
if (app_vars.uart_lastTxByte<sizeof(app_vars.uart_txFrame)) {
uart_writeByte(app_vars.uart_txFrame[app_vars.uart_lastTxByte]);
} else {
app_vars.uart_done=1;
}
}
void cb_uartRxCb(void) {
// uint8_t byte;
uart_clearRxInterrupts();
// toggle LED
leds_debug_toggle();
}
/**
\brief TelosB-specific definition of the "uart" bsp module.
\author Thomas Watteyne <watteyne@eecs.berkeley.edu>, February 2012.
*/
#include "msp430f1611.h"
#include "uart.h"
#include "board.h"
//=========================== defines =========================================
//=========================== variables =======================================
typedef struct {
uart_tx_cbt txCb;
uart_rx_cbt rxCb;
} uart_vars_t;
uart_vars_t uart_vars;
//=========================== prototypes ======================================
//=========================== public ==========================================
void uart_init() {
P3SEL |= 0xc0; // P3.6,7 = UART1TX/RX
UCTL1 = SWRST; // hold UART1 module in reset
UCTL1 |= CHAR; // 8-bit character
/*
// 9600 baud, clocked from 32kHz ACLK
UTCTL1 |= SSEL0; // clocking from ACLK
UBR01 = 0x03; // 32768/9600 = 3.41
UBR11 = 0x00; //
UMCTL1 = 0x4A; // modulation
*/
// 115200 baud, clocked from 4.8MHz SMCLK
UTCTL1 |= SSEL1; // clocking from SMCLK
UBR01 = 41; // 4.8MHz/115200 - 41.66
UBR11 = 0x00; //
UMCTL1 = 0x4A; // modulation
ME2 |= UTXE1 + URXE1; // enable UART1 TX/RX
UCTL1 &= ~SWRST; // clear UART1 reset bit
}
void uart_setCallbacks(uart_tx_cbt txCb, uart_rx_cbt rxCb) {
uart_vars.txCb = txCb;
uart_vars.rxCb = rxCb;
}
void uart_enableInterrupts(){
IE2 |= (URXIE1 | UTXIE1);
}
void uart_disableInterrupts(){
IE2 &= ~(URXIE1 | UTXIE1);
}
void uart_clearRxInterrupts(){
IFG2 &= ~URXIFG1;
}
void uart_clearTxInterrupts(){
IFG2 &= ~UTXIFG1;
}
void uart_writeByte(uint8_t byteToWrite){
U1TXBUF = byteToWrite;
}
uint8_t uart_readByte(){
return U1RXBUF;
}
//=========================== private =========================================
//=========================== interrupt handlers ==============================
kick_scheduler_t uart_tx_isr() {
uart_clearTxInterrupts(); // TODO: do not clear, but disable when done
uart_vars.txCb();
return DO_NOT_KICK_SCHEDULER;
}
kick_scheduler_t uart_rx_isr() {
uart_clearRxInterrupts(); // TODO: do not clear, but disable when done
uart_vars.rxCb();
return DO_NOT_KICK_SCHEDULER;
}