Part Number: TIDM-1002
Other Parts Discussed in Thread: MSP430FR5994
Tool/software: Code Composer Studio
Hello TI experts,
I am playing around with the TIDM-1002 Ultrasonic Gas Meter Front-End With MSP430 Reference design. I am trying to build the example project provided with the gasLibrary in Code Composer Studio, however, there seems to be a linking problem. I am attaching to this post a copy of the complete build log, while here you can find the problematic part:
'Invoking: MSP430 Linker' "C:/ti/ccsv7/tools/compiler/ti-cgt-msp430_16.9.6.LTS/bin/cl430" -vmspx --data_model=restricted -O3 --opt_for_speed=5 --use_hw_mpy=F5 --advice:power="none" --advice:hw_config=all --define=__MSP430FR5994__ --define=_MPU_ENABLE -g --printf_support=full --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 -z -m"msp-expfr5994_gas_afe_bp_fire_capture_processing.map" --heap_size=160 --stack_size=160 --cinit_hold_wdt=on -i"C:/ti/ccsv7/ccs_base/msp430/include" -i"C:/ti/ccsv7/ccs_base/msp430/lib/5xx_6xx_FRxx" -i"C:/ti/ccsv7/ccs_base/msp430/lib/FR59xx" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-msp430_16.9.6.LTS/lib" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-msp430_16.9.6.LTS/include" --priority --reread_libs --define=_MPU_ENABLE --diag_wrap=off --display_error_number --warn_sections --xml_link_info="msp-expfr5994_gas_afe_bp_fire_capture_processing_linkInfo.xml" --use_hw_mpy=F5 --rom_model -o "msp-expfr5994_gas_afe_bp_fire_capture_processing.out" "./hmi.obj" "./main.obj" "./GASMeteringLibraryConfig/gasMeteringUserConfig.obj" "./common/gui/GUI_Comm.obj" "./common/gui/TI_SerialComm.obj" "./common/gui/hal_uart.obj" "./common/hal/msp430fr5xx_6xx/gasMeteringHAL.obj" "./common/hal/msp430fr5xx_6xx/hal.obj" "./common/hal/msp430fr5xx_6xx/hal_adc.obj" "./common/hal/msp430fr5xx_6xx/hal_clk.obj" "./common/hal/msp430fr5xx_6xx/hal_dma.obj" "./common/hal/msp430fr5xx_6xx/hal_gpio.obj" "./common/hal/msp430fr5xx_6xx/hal_spi.obj" "./common/hal/msp430fr5xx_6xx/hal_timer.obj" "./common/hal/msp430fr5xx_6xx/hmiHAL.obj" "./driverlib/MSP430FR5xx_6xx/adc12_b.obj" "./driverlib/MSP430FR5xx_6xx/aes256.obj" "./driverlib/MSP430FR5xx_6xx/comp_e.obj" "./driverlib/MSP430FR5xx_6xx/crc.obj" "./driverlib/MSP430FR5xx_6xx/crc32.obj" "./driverlib/MSP430FR5xx_6xx/cs.obj" "./driverlib/MSP430FR5xx_6xx/dma.obj" "./driverlib/MSP430FR5xx_6xx/esi.obj" "./driverlib/MSP430FR5xx_6xx/eusci_a_spi.obj" "./driverlib/MSP430FR5xx_6xx/eusci_a_uart.obj" "./driverlib/MSP430FR5xx_6xx/eusci_b_i2c.obj" "./driverlib/MSP430FR5xx_6xx/eusci_b_spi.obj" "./driverlib/MSP430FR5xx_6xx/framctl.obj" "./driverlib/MSP430FR5xx_6xx/framctl_a.obj" "./driverlib/MSP430FR5xx_6xx/gpio.obj" "./driverlib/MSP430FR5xx_6xx/lcd_c.obj" "./driverlib/MSP430FR5xx_6xx/mpu.obj" "./driverlib/MSP430FR5xx_6xx/mpy32.obj" "./driverlib/MSP430FR5xx_6xx/pmm.obj" "./driverlib/MSP430FR5xx_6xx/ram.obj" "./driverlib/MSP430FR5xx_6xx/ref_a.obj" "./driverlib/MSP430FR5xx_6xx/rtc_b.obj" "./driverlib/MSP430FR5xx_6xx/rtc_c.obj" "./driverlib/MSP430FR5xx_6xx/sfr.obj" "./driverlib/MSP430FR5xx_6xx/sysctl.obj" "./driverlib/MSP430FR5xx_6xx/timer_a.obj" "./driverlib/MSP430FR5xx_6xx/timer_b.obj" "./driverlib/MSP430FR5xx_6xx/tlv.obj" "./driverlib/MSP430FR5xx_6xx/wdt_a.obj" "../lnk_msp430fr5994.cmd" -llibmpu_init.a -l"C:/ti/msp/gasLibrary_1_10_00_11/lib/gasMetering/CCS/gasMetering.a" -llibmath.a -llibc.a <Linking> undefined first referenced symbol in file --------- ---------------- LEASCCMA C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<leasc.o> LEASCCMCTL C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> LEASCCNF0 C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> LEASCCNF1 C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> LEASCCNF2 C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> LEASCIE C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> LEASCMT C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> LEASCPMCB C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibMeasurement.o> LEASCPMCTL C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> LEASCPMDST C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> LEASCPMS0 C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> LEASCPMS1 C:\ti\msp\gasLibrary_1_10_00_11\lib\gasMetering\CCS\gasMetering_CCS_large_code_restricted_data.lib<gasMeteringLibConfig.o> error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "msp-expfr5994_gas_afe_bp_fire_capture_processing.out" not built
As you can see, many symbols referenced in the gas Library are undefined. Since the gas library code is proprietary, I do not know how to solve this issue, because I have no idea where these definitions could be located. Can you help me find them?
I am using:
- GasLibrary_1_10_00_11 and I am trying to build its example project msp-expfr5994_gas_afe_bp
- Code Composer Studio 7.4.0.00015.
- Windows 7 x64
Compilation and linking options are the ones defined in the example project, I have not changed anything. However I am also attaching a BuildConfig.txt file in which I have copied all command line options as given to me by CCS in project properties.
Compiler Flags: -vmspx --data_model=restricted -O3 --opt_for_speed=5 --use_hw_mpy=F5 --include_path="C:/ti/ccsv7/ccs_base/msp430/include" --include_path="D:/LabMet/Desktop/CCSLocalWorkspace/msp-expfr5994_gas_afe_bp_fire_capture_processing" --include_path="D:/LabMet/Desktop/CCSLocalWorkspace/msp-expfr5994_gas_afe_bp_fire_capture_processing/common/gui" --include_path="D:/LabMet/Desktop/CCSLocalWorkspace/msp-expfr5994_gas_afe_bp_fire_capture_processing/common/hal/msp430fr5xx_6xx" --include_path="D:/LabMet/Desktop/CCSLocalWorkspace/msp-expfr5994_gas_afe_bp_fire_capture_processing/driverlib/MSP430FR5xx_6xx" --include_path="D:/LabMet/Desktop/CCSLocalWorkspace/msp-expfr5994_gas_afe_bp_fire_capture_processing/GASMeteringLibraryConfig" --include_path="C:/ti/msp/gasLibrary_1_10_00_11/include" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-msp430_16.9.6.LTS/include" --advice:power="none" --advice:hw_config=all --define=__MSP430FR5994__ --define=_MPU_ENABLE -g --printf_support=full --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 Linker Flags: -vmspx --data_model=restricted -O3 --opt_for_speed=5 --use_hw_mpy=F5 --advice:power="none" --advice:hw_config=all --define=__MSP430FR5994__ --define=_MPU_ENABLE -g --printf_support=full --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 -z -m"msp-expfr5994_gas_afe_bp_fire_capture_processing.map" --heap_size=160 --stack_size=160 --cinit_hold_wdt=on -i"C:/ti/ccsv7/ccs_base/msp430/include" -i"C:/ti/ccsv7/ccs_base/msp430/lib/5xx_6xx_FRxx" -i"C:/ti/ccsv7/ccs_base/msp430/lib/FR59xx" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-msp430_16.9.6.LTS/lib" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-msp430_16.9.6.LTS/include" --priority --reread_libs --define=_MPU_ENABLE --diag_wrap=off --display_error_number --warn_sections --xml_link_info="msp-expfr5994_gas_afe_bp_fire_capture_processing_linkInfo.xml" --use_hw_mpy=F5 --rom_model