This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EZ430-CHRONOS: 868MHZ access point connection problem

Part Number: EZ430-CHRONOS

Hello,

I have a eZ430 chronos 868 watch (white board access point) and I'm using windows XP sp3 operating system for compatibility. When I plug in the RF access point USB it flashes the led, the device is recognized. After that I started the control center, turned on the start access point and also started it in my watch by going to ACC then pressing down arrow. For a second it says getting data and then suddenly it says "RF Access Point Removed Press OK to close". After this my watch resets and battery becomes 3.01 V.( It charges back to 3.25 V after a few min). The control center closes but the led on the USB kept on. I tray to other windows vesions win7, win10 etc but problem persists. What can I do? please help me.

**Attention** This is a public forum