Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hello
I am new to CCS and MSP432 as well. I'm trying to communicate with the MPU6050 using the EUSCI-B0 module. I have the following connections in hardware:
* ACLK = n/a, MCLK = HSMCLK = SMCLK = BRCLK = default DCO = ~3.0MHz * * /|\ /|\ * MPU6050 4.7k 4.7k MSP432P401 * slave | | master * ----------------- | | ----------------- * | SDA|<-|----+->|P1.6/UCB3SDA | * | | | | | * | | | | | * | SCL|<-+------>|P1.7/UCB3SCL | * | | | | * "forum.43oh.com/.../"
/* DriverLib Includes */
#include <ti/devices/msp432p4xx/driverlib/driverlib.h>
/* Standard Includes */
#include <stdint.h>
#include <stdbool.h>
#include <printf.h>
#include <time.h>
#define RED 255
#define GREEN 255
#define BLUE 255
#define MCLK_FREQUENCY 12000000
#define PWM_PERIOD (MCLK_FREQUENCY/5000)
#define SLAVE_ADDRESS 0x68
#define NUM_OF_REC_BYTES 14
/* UART Configuration Parameter. These are the configuration parameters to
* make the eUSCI A UART module to operate with a 9600 baud rate. These
* values were calculated using the online calculator that TI provides
* at:
*software-dl.ti.com/.../index.html
*/
/* Statics for I2C working with the MPU6050 sensor*/
int i = 0;
uint8_t TXData[16] = {0x6B,0x00,0x3B,0x3C,0x3D,0x3E,0x3F,0x40,0x41,0x42,0x43,0x44,0x45,0x46,0x47,0x48};
static uint8_t RXData[NUM_OF_REC_BYTES];
static volatile bool stopSent;
static uint8_t TXByteCtr;
unsigned int iter=0;
void EUSCIA0_IRQHandler(void);
const uint8_t port_mapping[] =
{
//Port P2:
PM_TA0CCR1A, PM_TA0CCR2A, PM_TA0CCR3A, PM_NONE, PM_TA1CCR1A, PM_NONE, PM_NONE, PM_NONE
};
const eUSCI_UART_Config uartConfig =
{
EUSCI_A_UART_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
78, // BRDIV = 78
2, // UCxBRF = 2
0, // UCxBRS = 0
EUSCI_A_UART_NO_PARITY, // No Parity
EUSCI_A_UART_LSB_FIRST, // MSB First
EUSCI_A_UART_ONE_STOP_BIT, // One stop bit
EUSCI_A_UART_MODE, // UART mode
EUSCI_A_UART_OVERSAMPLING_BAUDRATE_GENERATION // Oversampling
};
/* I2C Master Configuration Parameter */
const eUSCI_I2C_MasterConfig i2cConfig =
{
EUSCI_B_I2C_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
3000000, // SMCLK = 3MHz
EUSCI_B_I2C_SET_DATA_RATE_100KBPS, // Desired I2C Clock of 100khz
0, // No byte counter threshold
EUSCI_B_I2C_NO_AUTO_STOP // No Autostop
};
int main(void){
/* Halting WDT and disabling master interrupts */
MAP_WDT_A_holdTimer();
//MAP_Interrupt_disableMaster();
/* Setting DCO to 12MHz */
//CS_setDCOCenteredFrequency(CS_DCO_FREQUENCY_12);
// Set P1.0 to output direction
GPIO_setAsOutputPin(
GPIO_PORT_P1,
GPIO_PIN0
);
MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
/* Selecting P1.2 and P1.3 in UART mode and P1.0 as output (LED) */
MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,
GPIO_PIN1 |GPIO_PIN2 | GPIO_PIN3, GPIO_PRIMARY_MODULE_FUNCTION);
/* Selecting P3.2 and P3.3 in UART mode */
MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P3,
GPIO_PIN2 | GPIO_PIN3, GPIO_PRIMARY_MODULE_FUNCTION);
/* Select Port 1 for I2C - Set Pin 6, 7 to Secondary Module Function,
* (UCB3SIMO/UCB3SDA, UCB3SOMI/UCB3SCL).
*/
MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,
GPIO_PIN6 + GPIO_PIN7, GPIO_PRIMARY_MODULE_FUNCTION);
/* Initialize main clock to 12MHz */
MAP_CS_setDCOCenteredFrequency(CS_DCO_FREQUENCY_12);
MAP_CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
MAP_CS_initClockSignal(CS_HSMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
MAP_CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
/* Configuring UART Module */
MAP_UART_initModule(EUSCI_A0_BASE, &uartConfig);
MAP_UART_initModule(EUSCI_A2_BASE, &uartConfig);
/* Initializing I2C Master to SMCLK at 400khz with no autostop */
MAP_I2C_initMaster(EUSCI_B0_BASE, &i2cConfig);
/* Specify slave address */
MAP_I2C_setSlaveAddress(EUSCI_B0_BASE, SLAVE_ADDRESS);
/* Set Master in transmit mode */
MAP_I2C_setMode(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_MODE);
/* Enable UART module */
MAP_UART_enableModule(EUSCI_A0_BASE);
MAP_UART_enableModule(EUSCI_A2_BASE);
//UART_registerInterrupt(EUSCI_A0_BASE, EUSCIA0_IRQHandler);
/* Enable I2C Module to start operations */
MAP_I2C_enableModule(EUSCI_B0_BASE);
/* GPIO Setup for Pins 2.0-2.2 */
MAP_PMAP_configurePorts((const uint8_t *) port_mapping, PMAP_P2MAP, 1,
PMAP_DISABLE_RECONFIGURATION);
MAP_GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P2,
GPIO_PIN0 | GPIO_PIN1 | GPIO_PIN2, GPIO_PRIMARY_MODULE_FUNCTION);
/* Confinguring P1.1 & P1.4 as an input and enabling interrupts */
MAP_GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN1 | GPIO_PIN4);
MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, GPIO_PIN1 | GPIO_PIN4);
MAP_GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN1 | GPIO_PIN4);
MAP_GPIO_interruptEdgeSelect(GPIO_PORT_P1, GPIO_PIN1 | GPIO_PIN4, GPIO_HIGH_TO_LOW_TRANSITION);
/* Configure TimerA0 without Driverlib (CMSIS style register access) */
TIMER_A0->CCR[0] = PWM_PERIOD;
TIMER_A0->CCTL[1] = TIMER_A_CCTLN_OUTMOD_7; // CCR1 reset/set
TIMER_A0->CCR[1] = PWM_PERIOD * (RED/255); // CCR1 PWM duty cycle
TIMER_A0->CCTL[2] = TIMER_A_CCTLN_OUTMOD_7; // CCR2 reset/set
TIMER_A0->CCR[2] = PWM_PERIOD * (0/255); // CCR2 PWM duty cycle
TIMER_A0->CCTL[3] = TIMER_A_CCTLN_OUTMOD_7; // CCR3 reset/set
TIMER_A0->CCR[3] = PWM_PERIOD * (0/255); // CCR3 PWM duty cycle
TIMER_A0->CTL = TIMER_A_CTL_SSEL__SMCLK | TIMER_A_CTL_MC__UP | TIMER_A_CTL_CLR; // SMCLK, up mode, clear TAR
/* Configure and enable SysTick */
MAP_SysTick_setPeriod(1500000);
MAP_SysTick_enableModule();
MAP_SysTick_enableInterrupt();
MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, GPIO_PIN1 | GPIO_PIN4);
MAP_Interrupt_enableInterrupt(INT_PORT1);
/* Enable and clear the interrupt flag */
MAP_I2C_clearInterruptFlag(EUSCI_B0_BASE,
EUSCI_B_I2C_TRANSMIT_INTERRUPT0 + EUSCI_B_I2C_NAK_INTERRUPT);
/* Enabling interrupts */
MAP_UART_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT | EUSCI_A_UART_RECEIVE_ERRONEOUSCHAR_INTERRUPT
| EUSCI_A_UART_BREAKCHAR_INTERRUPT);
MAP_UART_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT);
//MAP_UART_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_TRANSMIT_INTERRUPT);
MAP_UART_enableInterrupt(EUSCI_A2_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT);
//enable interrupts for each module
MAP_Interrupt_enableInterrupt(INT_EUSCIA0);
MAP_Interrupt_enableInterrupt(INT_EUSCIA2);
MAP_Interrupt_enableInterrupt(INT_EUSCIB0);
//MAP_Interrupt_enableSleepOnIsrExit();
MAP_Interrupt_enableMaster();
TXData[0] = 0x3B;
printf(EUSCI_A0_BASE, "Tx: %x\n\r", TXData[0]);
//MAP_I2C_masterSendMultiByteStart(EUSCI_B0_BASE, TXData[0]);
//MAP_I2C_masterSendMultiByteStopWithTimeout(EUSCI_B0_BASE, 1000); //Chosen arbitrary value for timeout
MAP_I2C_masterSendSingleByte(EUSCI_B0_BASE, TXData[0]);
//while (I2C_isBusBusy(EUSCI_B0_BASE)==EUSCI_B_I2C_BUS_BUSY);
MAP_I2C_enableInterrupt(EUSCI_B0_BASE,EUSCI_B_I2C_RECEIVE_INTERRUPT0);
while (MAP_I2C_masterIsStopSent(EUSCI_B0_BASE) == EUSCI_B_I2C_SENDING_STOP);
//while(!UCB0IFG);
MAP_I2C_masterReceiveStart(EUSCI_B0_BASE);
while(1)
{
printf(EUSCI_A0_BASE, "Main started \n\r");
MAP_PCM_gotoLPM0InterruptSafe();
//MAP_PCM_gotoLPM0();
}
}
void EUSCIB0_IRQHandler(void)
{
uint_fast16_t status;
status = MAP_I2C_getEnabledInterruptStatus(EUSCI_B0_BASE);
MAP_I2C_clearInterruptFlag(EUSCI_B0_BASE, status);
//printf(EUSCI_A0_BASE, "I2C\n\r");
if (status & EUSCI_B_I2C_TRANSMIT_INTERRUPT0)
{
printf(EUSCI_A0_BASE, "I2C_Sent!\n\r");
//MAP_I2C_disableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_INTERRUPT0);
//MAP_I2C_disableModule(EUSCI_B0_BASE);
//MAP_I2C_setMode(EUSCI_B0_BASE, EUSCI_B_I2C_RECEIVE_MODE);
//MAP_I2C_enableModule(EUSCI_B0_BASE);
//MAP_I2C_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_RECEIVE_INTERRUPT0);
//MAP_I2C_masterReceiveStart(EUSCI_B0_BASE);
}
if (status & EUSCI_B_I2C_RECEIVE_INTERRUPT0)
{
RXData[0] = MAP_I2C_masterReceiveMultiByteNext(
EUSCI_B0_BASE);
printf(EUSCI_A0_BASE, "Finished receive: %x\n\r", RXData[0]);
//int i=iter - 2;
//printf(EUSCI_A0_BASE, "Iter: %i\r\n", iter);
//if(iter < 15)
{
//RXData[i] = MAP_I2C_masterReceiveMultiByteNext(EUSCI_B0_BASE);
//printf(EUSCI_A0_BASE, "Rec: %i\r\n", RXData[i]);
}
//else
{
// RXData[0] = MAP_I2C_masterReceiveSingleByte(EUSCI_B0_BASE);
//MAP_I2C_disableInterrupt(EUSCI_B0_BASE, EUSCI_B_I2C_RECEIVE_INTERRUPT0);
// printf(EUSCI_A0_BASE, "Finished receive: %x\n\r", RXData[0]);
}
//MAP_I2C_setMode(EUSCI_B0_BASE, EUSCI_B_I2C_TRANSMIT_MODE);
// stopSent = true;
}
}
/* EUSCI A0 UART ISR - Echoes data back to PC host */
void EUSCIA0_IRQHandler(void)
{
//char receiveByte = UCA0RXBUF;
uint32_t status = MAP_UART_getEnabledInterruptStatus(EUSCI_A0_BASE);
MAP_UART_clearInterruptFlag(EUSCI_A0_BASE, status);
if(EUSCI_A_UART_RECEIVE_INTERRUPT_FLAG)
{
MAP_UART_transmitData(EUSCI_A0_BASE, MAP_UART_receiveData(EUSCI_A0_BASE));
}
}
/* EUSCI A2 UART ISR - Echoes data back to PC host */
void EUSCIA2_IRQHandler(void)
{
uint32_t status = MAP_UART_getEnabledInterruptStatus(EUSCI_A2_BASE);
MAP_UART_clearInterruptFlag(EUSCI_A2_BASE, status);
if(status & EUSCI_A_UART_RECEIVE_INTERRUPT_FLAG)
{
printf(EUSCI_A0_BASE, "Receive2\n\r");
}
if(status & EUSCI_A_UART_TRANSMIT_INTERRUPT_FLAG)
{
printf(EUSCI_A0_BASE, "Transmit2 \n\r");
}
}
/*
* Port 1 interrupt handler. This handler is called whenever switches attached
* to P1.1 (S1) and P1.4 (S2) are pressed.
*/
void PORT1_IRQHandler(void)
{
//newTick = MAP_SysTick_getValue();
uint32_t status = MAP_GPIO_getEnabledInterruptStatus(GPIO_PORT_P1);
MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, status);
/* Handles S1 button press */
if (status & GPIO_PIN1)
{
//MAP_Interrupt_disableInterrupt(INT_PORT1);
printf(EUSCI_A0_BASE, "LED should light up \n\r");
TIMER_A0->CCR[1] = PWM_PERIOD * (0/255); // CCR1 PWM duty cycle
TIMER_A0->CCR[2] = PWM_PERIOD * (GREEN/255); // CCR2 PWM duty cycle
TIMER_A0->CCR[3] = PWM_PERIOD * (0/255); // CCR3 PWM duty cycle
MAP_GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
printf(EUSCI_A0_BASE, "LED lit?");
}
/* Handles S2 button press */
if (status & GPIO_PIN4)
{
/* Initialize values to display */
char *s = "printf test";
char c = '!';
int i = -12345;
unsigned u = 4321;
long int l = -123456780;
long unsigned n = 1098765432;
unsigned x = 0xABCD;
printf(EUSCI_A0_BASE, "String %s\r\n", s);
printf(EUSCI_A0_BASE, "Char %c\r\n", c);
printf(EUSCI_A0_BASE, "Integer %i\r\n", i);
printf(EUSCI_A0_BASE, "Unsigned %u\r\n", u);
printf(EUSCI_A0_BASE, "Long %l\r\n", l);
printf(EUSCI_A0_BASE, "uNsigned loNg %n\r\n", n);
printf(EUSCI_A0_BASE, "heX %x\r\n", x);
}
}
/*
* SysTick interrupt handler. This handler toggles RGB LED on/off.
*/
void SysTick_Handler(void)
{
if (!(TIMER_A0->CCTL[1] & TIMER_A_CCTLN_OUTMOD_0)){
TIMER_A0->CCTL[1] = TIMER_A_CCTLN_OUTMOD_7;
TIMER_A0->CCTL[2] = TIMER_A_CCTLN_OUTMOD_7;
TIMER_A0->CCTL[3] = TIMER_A_CCTLN_OUTMOD_7;
}
}