We are considering to use a MSP430FR2111 device for our application.
In this application we need to:
- sample a pin quickly (< 5ms) after power is applied.
- communicate with a host System (at 9600 or 19200 baud); we are still open for the used baudrate not yet defined
When sampling the IO port, the operating frequncy does not have to be preceise, but for the USART communication we do need to match the Baudrate within about 4%.
The DCO with FLL would meet the requirement with 2%. But the FLL lock time is specified with 245ms typical, which is to long.
The device descriptor (TLV) contains a DCO Calibration value.
- what tolerance does the DCO have when using this value
- will the FLL lock faster when starting with the DCO calibration value? (how Long will it take?)
Any ideas are welcome