Other Parts Discussed in Thread: MSP430FR5969, MSP430WARE
Tool/software: Code Composer Studio
I've encountered a problem when launching a program onto the launchpad. Please see the below screenshot. I'm using CCS version 7.01
Previously it worked very well. But lately I've used the onboard EZ-FET to launch the program onto another MSP430FR5969 target on my PCB. The first times it worked. I followed exactly the instruction at page 15, " Using the eZ-FET Emulator With a Different Target" with 6-wire connected between the launchpad and the target, including V+, GND, SBWTDIO (connected to pin RST of the target), SBWTCK (connected to pin TEST of the target). EZFET-UARTRXD (connected to TXD of the target), EZFET-UARTTXD (to the target TXD). For the first time, it did work. But then, I could not launch any program onto even the on-board MCU of the launchpad!
I lost the micro-usb cable of the pad long time ago, so I replaced it by the charging cable of my cell phone. It seems compatible because I successfully launched the program several times before that problem.
Any help would be highly appreciated.