Part Number: MSP430FR2433
Other Parts Discussed in Thread: MSP430G2553
I have recently ported an application from an MSP430G2553 to the MSP430FR2433. That has gone well and everything is working nicely with the newer MCU.
However, reading the data sheet for the new chip I see that SPI is specified to have a maximum clock frequency of 8MHz. I'm running MCLK and SMCLK at 12MHz and am running the eUSCI clock without a divider. SPI output (which is used quite heavily) is working fine at 12MHz, and looks fine on the oscilloscope. I'm reluctant to divide it down to 6MHz.
The old chip's data sheet said its SPI could handle anything up to MCLK. It is unusual for a newer chip to claim poorer performance. Was it just TI being conservative or will I face real reliability problems running at 12MHz?
Thanks.