Other Parts Discussed in Thread: ENERGIA, UNIFLASH, MSP-EXP430FR4133
I can no longer upload to the MSP-EXP430FR5994 when running on macOS 10.14 Mojave. Uploading to ezFET used to work fine with macOS 10.13 High Sierra.
- DSLite used with Energia fails to upload to the MSP-EXP430FR5994 LaunchPad.
DSLite version 8.2.0.1400Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: MSP430
error: MSP430: Error initializing emulator: No USB FET was found
Failed: MSP430: Error initializing emulator: No USB FET was foundthe selected serial port
does not exist or your board is not connected
The issue has been reported as macOS 10.14 — Upload to MSP430FR5994 Fails #69.
- Command line MSP430Flasher fails to detect the ezFET.
$ ./MSP430Flasher -i usbmodem* * -----/|-------------------------------------------------------------------- * * / |__ * * /_ / MSP Flasher v1.3.16 * * | / * * -----|/-------------------------------------------------------------------- * * * Evaluating triggers...done * Checking for available FET debuggers: * Couldn't find any connected USB FETs! * Powering down...done * Disconnecting from device...done * * ---------------------------------------------------------------------------- * Driver : closed (MSP DebugStack not initialized) * ---------------------------------------------------------------------------- */
- Same result with CCS Cloud.
An error message appears about El Capitan on macOS 10.12, which is two year old. macOS 10.14 Mojave has just been released.
- Finally, UniFlash fails as well.
Any solution? Thank you!