This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432P4111: MSP432P4111 + EnergyTrace error

Part Number: MSP432P4111
Other Parts Discussed in Thread: ENERGYTRACE

Tool/software: Code Composer Studio

Hello

I am doing SimpleLink academy lab "SimpleLink SDK - LaunchPad Power Measurements Using EnergyTrace™" on MSP432P4111 launchpad and at Task 5 I got problem. I run "powerdeepsleep" example with debugger, when red LED turned on I press S1 button, red LED turn off and I turn on EnergyTrace to measure current but when I press green button it says that maximum current limit is 75mA and stops working(EnergyTrace is configured as it is shown in Task 4). when I press green button again it runs and never stops (Timeout is set to 10 sec). I try to configure EnergyTrace for higher currents but everything is same. I have no idea what to do now. can anyone help me?

Thanks.

**Attention** This is a public forum