Part Number: MSP430F2272
Other Parts Discussed in Thread: UNIFLASH
Dear all,
one of my AA is experiencing some issue with the MSP430F2272IRHAT. In particular the data in the flash are get corrupted. The application is and hand held radio and the suspect is that during the replacement of the battery the uC can experience noisy voltage supply.
In order to mitigate the corruption of the data, the designers would put the reset pin with a pull down to 0V regardless to the voltage supply of the uC and remove the device from reset after the complete turn on of the radio. Can this procedure help in the protection of the data in the flash ?
Do you have any other suggestions ? Consider that the radio has been produces since 2007 and only in the last years they have experienced a lot of returns from the customers.
regards,
Domenico