Part Number: MSP430FR2433
Other Parts Discussed in Thread: MSP430WARE
Hi all, I am trying to transmit data from microcontroller to pc by running uscia0 in uart mode. I took an example from msp430ware and modified to send a character to pc when a push button pressed. But I can't see any data on my PC.
PC side I am using Linux host with putty. and I am looking at the port ttyACM1 (Not sure which of ttyACM1 and ttyACM0 to check). I am including entire code below. Kindly notify me if I am doing any mistake in the implementation.
Thanks,
Ravi.\
/////////////////////////////////////////////////////// code /////////
#include <msp430.h>
#define MCLK_FREQ_MHZ 8 // MCLK = 8MHz
void Software_Trim();
void Init_GPIO();
volatile unsigned int p=0;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
// Configure GPIO
Init_GPIO();
PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode
// to activate 1previously configured port settings
__bis_SR_register(SCG0); // disable FLL
CSCTL3 |= SELREF__REFOCLK; // Set REFO as FLL reference source
CSCTL1 = DCOFTRIMEN | DCOFTRIM0 | DCOFTRIM1 | DCORSEL_3;// DCOFTRIM=3, DCO Range = 8MHz
CSCTL2 = FLLD_0 + 243; // DCODIV = 8MHz
__delay_cycles(3);
__bic_SR_register(SCG0); // enable FLL
Software_Trim(); // Software Trim to get the best DCOFTRIM value
CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK; // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
// default DCODIV as MCLK and SMCLK source
// Configure UART pins
P1SEL0 |= BIT4 | BIT5; // set 2-UART pin as second function
// Configure UART
UCA0CTLW0 |= UCSWRST;
UCA0CTLW0 |= UCSSEL__SMCLK;
// Baud Rate calculation
// 8000000/(16*9600) = 52.083
// Fractional portion = 0.083
// User's Guide Table 14-4: UCBRSx = 0x49
// UCBRFx = int ( (52.083-52)*16) = 1
UCA0BR0 = 52; // 8000000/16/9600
UCA0BR1 = 0x00;
UCA0MCTLW = 0x4900 | UCOS16 | UCBRF_1;
UCA0STATW |= 0x0080;
UCA0CTLW0 &= ~UCSWRST; // Initialize eUSCI
while(1)
{
if (!(P2IN & BIT3))
{
if(p==0)
{
UCA0TXBUF = 1 ; // P1.0 TOGGLE
__no_operation();
p=1;
}
}
else
p = 0;
}
}
void Init_GPIO()
{
P1DIR = 0xFF; P3DIR = 0xFF;
P1REN = 0xFF; P3REN = 0xFF;
P1OUT = 0x00; P3OUT = 0x00;
P2DIR |= BIT3; // Set P2.3 to input direction
P2REN |= BIT3; // P2.3 Enable pull-up resistors
P2OUT |= BIT3; // Configure P2.3 pull-up
}
void Software_Trim()
{
unsigned int oldDcoTap = 0xffff;
unsigned int newDcoTap = 0xffff;
unsigned int newDcoDelta = 0xffff;
unsigned int bestDcoDelta = 0xffff;
unsigned int csCtl0Copy = 0;
unsigned int csCtl1Copy = 0;
unsigned int csCtl0Read = 0;
unsigned int csCtl1Read = 0;
unsigned int dcoFreqTrim = 3;
unsigned char endLoop = 0;
do
{
CSCTL0 = 0x100; // DCO Tap = 256
do
{
CSCTL7 &= ~DCOFFG; // Clear DCO fault flag
}while (CSCTL7 & DCOFFG); // Test DCO fault flag
__delay_cycles((unsigned int)3000 * MCLK_FREQ_MHZ);// Wait FLL lock status (FLLUNLOCK) to be stable
// Suggest to wait 24 cycles of divided FLL reference clock
while((CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)) && ((CSCTL7 & DCOFFG) == 0));
csCtl0Read = CSCTL0; // Read CSCTL0
csCtl1Read = CSCTL1; // Read CSCTL1
oldDcoTap = newDcoTap; // Record DCOTAP value of last time
newDcoTap = csCtl0Read & 0x01ff; // Get DCOTAP value of this time
dcoFreqTrim = (csCtl1Read & 0x0070)>>4;// Get DCOFTRIM value
if(newDcoTap < 256) // DCOTAP < 256
{
newDcoDelta = 256 - newDcoTap; // Delta value between DCPTAP and 256
if((oldDcoTap != 0xffff) && (oldDcoTap >= 256)) // DCOTAP cross 256
endLoop = 1; // Stop while loop
else
{
dcoFreqTrim--;
CSCTL1 = (csCtl1Read & (~(DCOFTRIM0+DCOFTRIM1+DCOFTRIM2))) | (dcoFreqTrim<<4);
}
}
else // DCOTAP >= 256
{
newDcoDelta = newDcoTap - 256; // Delta value between DCPTAP and 256
if(oldDcoTap < 256) // DCOTAP cross 256
endLoop = 1; // Stop while loop
else
{
dcoFreqTrim++;
CSCTL1 = (csCtl1Read & (~(DCOFTRIM0+DCOFTRIM1+DCOFTRIM2))) | (dcoFreqTrim<<4);
}
}
if(newDcoDelta < bestDcoDelta) // Record DCOTAP closest to 256
{
csCtl0Copy = csCtl0Read;
csCtl1Copy = csCtl1Read;
bestDcoDelta = newDcoDelta;
}
}while(endLoop == 0); // Poll until endLoop == 1
CSCTL0 = csCtl0Copy; // Reload locked DCOTAP
CSCTL1 = csCtl1Copy; // Reload locked DCOFTRIM
while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked
}