Part Number: MSP430FR2433
Hi, I'm trying to use DCO without FLL operation. Is is possbile without problem over temperature?
The DCO FLL lock time of MSP430FR2433 is described as 280ms at the datasheet.
It is too late for our application and 2ms is desired.
In order to solve the issue, is it possbile for us to do the following usage?
1) At a factory, CSCTLO register value is measured using FLL operation under 25 °C
2) Then, the measured value is stored to the FeRAM.
3) When the MSP430FR2433 is powered on, it reads the value for CSCTL0 from the FeRAM
and then the value is set to the CSCTL0 register.
4) After setting the CSCTL0 value, we force MSP430FR2433 not to use FLL.
5) The product may be used from -10°C to +60°C.
I have another question.
Without FLL operation, Could we think that the DCO frequency torelance is
same as REFO absolute calibrated tolerance( –40°C to 85°C 1.8 V to 3.6 V) –3.5% +3.5%?