Part Number: MSP-TS430RHA40A
Other Parts Discussed in Thread: MSP430FR5739, MSP-FET, MSP430FR5738,
Hi,
I have a weird problem when trying to flash/program the MSP430FR5739 using SBW with CCS. The devkit JP4 to JP9 being placed on 1-2 for SBW. C5 is DNP. The program only flashes with JTAG or an older version of the MSP-FET.
I have two versions of the MSP-FET, the latest edition with serial 1805002D7 has an issue when trying to flash the code using CCS, I am getting:
"Error connecting to target: unknown device" (only when using SBW)
The older version of the MSP-FET is uploading the code, but it is not always able to connect. Sometimes it refuses to connect at all.
Fore more information the JTAG is working fine, I need SBW to work and I am not sure what is causing the issue, I have a prototype that is using the MSP430FR5738 and it is having exactly the same problem.