Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/MSP432E401Y: mqtt client blocks http server

Part Number: MSP432E401Y

Tool/software: TI-RTOS

Hi all,

I want to run a http server in parallel to a mqtt client on the MSP432E401 using the simplelink sdk. I used these examples to combine into one project:

  • SimpleLink MSP432E4 SDK-SysConfig Preview-Network Services-httpserver
  • SimpleLink MSP432E4 SDK-SysConfig Preview-Network Services-mqttclient

Both threads start as planned, but the mqtt client now blocks the http server. No access to http is possible.

Doing a suspend in the debugger reveals that the MCU is locked in this loop (see yellow below) in mqtt_client_app.c in function "mainThread":

...

 while (1)
    {
        gResetApplication = false;
        topic[0] = SUBSCRIPTION_TOPIC0;
        topic[1] = SUBSCRIPTION_TOPIC1;
        gInitState = 0;
        /* Connect to AP                                                      */
        gApConnectionState = Mqtt_IF_Connect();
        gInitState |= MQTT_INIT_STATE;
        /* Run MQTT Main Thread (it will open the Client and Server)          */
        Mqtt_start();
        /* Wait for init to be completed!!!                                   */
        while (gInitState != 0)
        {
            Display_printf(display, 0, 0, ".");
            sleep(1);
        }
        Display_printf(display, 0, 0, ".");
        while (gResetApplication == false);
        Display_printf(display, 0, 0,
                "TO Complete - Closing all threads and resources");
        /* Stop the MQTT Process                                              */
        Mqtt_Stop();
        Display_printf(display, 0, 0, "reopen MQTT # %d  ", ++count);
    }

...

I changed the marked code to:

while (gResetApplication == false) {
     TaskSleep(50);
}

This seems to help, but is this intended? Is there a better way to do it? If TaskSleep is the way to go, is there a recommended value for the delay parameter?

Thanks & best regards,
Christian Seidel

**Attention** This is a public forum