Part Number: MSP430F5437A
Hello,
I will use this part(MSP430F5437A) for a commercial product.
I found the following information from MSP430 BSL.
If the device is secured by disabling JTAG, it is still possible to use the BSL. Access to the MSP430 MCU
memory through the BSL is protected against misuse by the BSL password.
Can this features of MSP430F5437A cover the following issues?
- protecting the flash from any external reading or modification after the production phase
- not being modified or overwritten on production phase
- no option for the chip start from an alternated code source
Thanks, HJ