Other Parts Discussed in Thread: UNIFLASH,
Hello,
I'm using the MSP-FET, together with the MSP-FET-432ADPTR , to program an MSP432P401R in a production line through UNIFLASH.
In my setup the MSP432 is not powered when first connected to the programming station. The operator has to press a button to turn on the voltages.
However, when connected to the MSP-FET, voltages appear on the MSP432 voltage rail even without turning on the power and causes an unexpected behavior.
The switch setting on the MSP-FET-432ADPTR is set to "sense", and "VCC tool" is not connected anywhere on my board. Somehow, the MSP-FET is powering the MSP432.
I think this is caused by the "RST" line which, according to the datasheet and to measurements, is being actively driven to +3.3V on power up and through internal protection diodes powers the device.
Is this indeed the case? Is there any way to change this power up configuration of the RST line?