This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529: EV2400

Part Number: MSP430F5529
Other Parts Discussed in Thread: EV2400, , BQSTUDIO

Hi,

I wanted check Through few things related to EV2400, which uses msp430f5529 IC. I have a msp430f5529 Launchpad. I want to use it as a USB-based PC Interface for Battery Fuel (Gas) Gauge Evaluation Module(EV2400).

1. What are the Hardware and Firmware steps to be changed before Communicating the launchpad with bqstudio?

2. There is a  EV2400 Firmware Updater v0.28 (Rev. A), If I am using only msp430f5529 launchpad alone what are the procedure to be followed in order to update the firmware/program into the launchpad?

3. Can the  msp430f5529  Launchpad after making the changes be used to communicate with Bqstudio?

  • Hi 

    #1 We have provide the all the schematic for MSP430F5529 launchpad and EV2400 you can compare them to see where to change in the  hardware. 

    I if the MSP430F5529 hardware is changed meet the EV2400  I think don't change any firmware .

    #2 you can download the firmware directly with the launchpad

    #3 I think that should work with it

**Attention** This is a public forum