Part Number: MSP432P401R
The linker file is msp432p401r.lds so how to make a change in that file or is there any other option available to change stack size from. like Project>>Properties then >>...................... because I can't find the same. Help me with this. this is the msp432p401r.lds file.
MEMORY
{
MAIN_FLASH (RX) : ORIGIN = 0x00000000, LENGTH = 0x00040000
INFO_FLASH (RX) : ORIGIN = 0x00200000, LENGTH = 0x00004000
SRAM_CODE (RWX): ORIGIN = 0x01000000, LENGTH = 0x00010000
SRAM_DATA (RW) : ORIGIN = 0x20000000, LENGTH = 0x00010000
}
REGION_ALIAS("REGION_TEXT", MAIN_FLASH);
REGION_ALIAS("REGION_BSS", SRAM_DATA);
REGION_ALIAS("REGION_DATA", SRAM_DATA);
REGION_ALIAS("REGION_STACK", SRAM_DATA);
REGION_ALIAS("REGION_HEAP", SRAM_DATA);
REGION_ALIAS("REGION_ARM_EXIDX", MAIN_FLASH);
REGION_ALIAS("REGION_ARM_EXTAB", MAIN_FLASH);
SECTIONS {
PROVIDE (_intvecs_base_address =
DEFINED(_intvecs_base_address) ? _intvecs_base_address : 0x0);
.intvecs (_intvecs_base_address) : AT (_intvecs_base_address) {
KEEP (*(.intvecs))
} > REGION_TEXT
PROVIDE (_vtable_base_address =
DEFINED(_vtable_base_address) ? _vtable_base_address : 0x20000000);
.vtable (_vtable_base_address) : AT (_vtable_base_address) {
KEEP (*(.vtable))
} > REGION_DATA
.text : {
CREATE_OBJECT_SYMBOLS
KEEP (*(.text))
*(.text.*)
. = ALIGN(0x4);
KEEP (*(.ctors))
. = ALIGN(0x4);
KEEP (*(.dtors))
. = ALIGN(0x4);
__init_array_start = .;
KEEP (*(.init_array*))
__init_array_end = .;
*(.init)
*(.fini*)
} > REGION_TEXT AT> REGION_TEXT
.rodata : {
*(.rodata)
*(.rodata.*)
} > REGION_TEXT AT> REGION_TEXT
.ARM.exidx : {
__exidx_start = .;
*(.ARM.exidx* .gnu.linkonce.armexidx.*)
__exidx_end = .;
} > REGION_ARM_EXIDX AT> REGION_ARM_EXIDX
.ARM.extab : {
*(.ARM.extab* .gnu.linkonce.armextab.*)
} > REGION_ARM_EXTAB AT> REGION_ARM_EXTAB
__etext = .;
.data : {
__data_load__ = LOADADDR (.data);
__data_start__ = .;
KEEP (*(.data))
KEEP (*(.data*))
. = ALIGN (4);
__data_end__ = .;
} > REGION_DATA AT> REGION_TEXT
.bss : {
__bss_start__ = .;
*(.shbss)
KEEP (*(.bss))
*(.bss.*)
*(COMMON)
. = ALIGN (4);
__bss_end__ = .;
} > REGION_BSS AT> REGION_BSS
.heap : {
__heap_start__ = .;
end = __heap_start__;
_end = end;
__end = end;
KEEP (*(.heap))
__heap_end__ = .;
__HeapLimit = __heap_end__;
} > REGION_HEAP AT> REGION_HEAP
.stack (NOLOAD) : ALIGN(0x8) {
_stack = .;
__stack = .;
KEEP(*(.stack))
} > REGION_STACK AT> REGION_STACK
}