This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438A: UART Max Frequency when using DCO

Part Number: MSP430F5438A

Hello,

According to the datasheet we can use ACLK, SMCLK or external UCLK with max frequency limited to fsytem (section 5.3).
If a 24MHz crystal will be used, does it mean that UART clock will be limited to 24 Mhz or is it possible to have higher speed using DCO?

Thank you.

  • slau208 MSP430x5xx MSP430x6xx Family User's Guide   32.3.9.1 Low-Frequency Baud-Rate Generation
    In this mode, the maximum USCI baud rate is one-third the UART source clock frequency BRCLK.

    Maximum rate with error free transfer, for MSP430F5xx is 25/3 = 8.333 Mbps.

    https://forum.43oh.com/topic/3413-msp430-uart-benchmark/

**Attention** This is a public forum