Part Number: MSP430G2553
Tool/software: Code Composer Studio
Hello everyone, I have a school project that asked me to make a morse code using the msp430g2553 controller and the CCS compiler. I am struggling with making my Dot and Dash Function timing to work correctly. My string I set to be "test" and when I run it, the controller only flashes 1 and then flashes 1 more time and stay on. Here are my morse code array:
char morse[][numCols]= {
(".-"),("-..."),("-.-."),("-.."),("."),("..-."),("--."),("...."),(".."),(".---"),
("-.-"),(".-.."),("--"),("-."),("---"),(".--."),("--.-"),
(".-."),("..."),("-"),("..-"),("...-"),(".--"),("-..-"),
("-.--"),("--.."),
(".----"),("..---"),("...--"),("....-"),("....."),("-...."),
("--..."),("---.."),("----."),("-----")};
void main(){
WDTCTL = WDTPW + WDTHOLD;
P1DIR |=0x41;
P1OUT &= 0xBE;
char str[] = "test";
for (;;){
if (i < strlen(str)){
for (i = 0; i < strlen(str); i++){
compareChars(str[i]);
}
} else {
break;
reset();
}
}}
Then my compareChars function (short version) where it will convert my string into lower case and also have a switch case that detect every alphabet and refer to the morse array I have created:
void compareChars(char c1){
int j,k;
if (c1 >= 'A'&& c1 <= 'Z')
{
c1 += 32;
}
switch(c1){
case 'a':
for (j = 0; j < numCols; j++){
if (morse[0][j] != '\0'){
ReadMorseAlphabet(morse[0][j]);
for (k = 5000; k > 0; k--); //to create a delay
}
}
break;
case 'b':
for (j = 0; j < numCols; j++){
if (morse[1][j] != '\0'){
ReadMorseAlphabet(morse[1][j]);
for (k = 5000; k > 0; k--); //to create a delay
}
}
break;
(ETC)
and my Dot and Dash Function and also the reset function where it will flashes green to reset:
void ReadMorseAlphabet(char morseCode){
switch (morseCode){
case '.':
dot();
break;
case '-':
dash();
break;
default:
break;
}
}
void dot(){
P1OUT ^= 0x40;
for(i=1; i<= 20000; i++){
;}
for(i=1; i<= 20000; i++){
;}
}
void dash()
{
for(i=1; i<= 20000; i++){
;}
P1OUT ^= 0x40;
for(i=1; i<= 20000; i++){
;}
for(i=1; i<= 20000; i++){
;}
for(i=1; i<= 20000; i++){
;}
}
void reset()
{
P1OUT ^= 0x01;
for(i=1; i<= 20000; i++);
}