Part Number: MSP430G2955
Other Parts Discussed in Thread: MSP-ISO, MSP-FET, MSP-EXP430FR2433
I've been working with MSP430 for 10 years and one thing bothers me: the debugging/programming link is not very stable.
For battery fed applications, there's usually no problem, but If there is a switching power supply, or when switching high currents/ voltages, the debugger loses the connection, crashes, breaks,...
I recently bought an MSP-ISO board, that uses a ISO1541DR chip to make the separation.
I hoped providing galvanic seperation between the MSP project board and the programmer would eliminate the problem.
Unfortunately, the board is not compatible with the MSP-FET that I am using: on the isolator board, there is a 150 Ohm pull-up on the SBWTDIO line, and the scope shows me the programmer cannot pull it low.
I was wondering if there is another isolation board available that is compatible with the MSP-FET?