Part Number: MSP430F6779
Hi there,
I'm attempting to change the baud rate of the EMDC program on MSP430F6779.
I've seen links to Page 1040, Table 39-5, in the "Family" user's guide:
www.ti.com/.../slau208q.pdf
I've also seen references to the UART Baud Rate Calculator:
software-dl.ti.com/.../index.html
However, I cannot replicate the parameters in the EMDC program:
#if (EM_SMCLK_FREQ_IN_HZ == 25165824) //250K Baud Rate @ 25MHz #define UART__PRESCALER (0x06) #define UART__FIRST_STAGE_MOD (0x03) #define UART__SECOND_STAGE_MOD (0x02)
Why does the calculator give me a different set of parameters?
The Family user-guide does not appear to have an SMCLK -> BRCLK value of 25165824 Hz in the table.
How do I calculate the parameters to get to... 9600 Baud, or 115200 Baud, or 400 kBaud?