This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430FR2355: MSP low-power microcontroller forum

Part Number: MSP-EXP430FR2355


Hello team,

I'm working with WDT and facing problem in configuring WDT for near to 15msec.

I want my clock to be 24Mhz WDT  reset timings is ~15msec for WDT can use any clock source. Please someone suggest in configuring WDT. 

I already tried with below code and failed. The behaviour of WDT is unpredictable. Someone explain me why? 

#include <msp430.h> 
void clock_setup(void);
int main(void)
{
    WDTCTL = WDTPW | WDTHOLD;                 // Stop WDT
    clock_setup();

    P1DIR |= BIT0;// Set P1.0 to output direction
    P6DIR |= BIT6;
    P1OUT ^= BIT0;

    PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode
                                 // to activate previously configured port settings

    WDTCTL = WDTPW | WDTSSEL_1 | WDTCNTCL | WDTTMSEL_0 | WDTIS_6;                   // WDT 32ms, SMCLK, interval timer


 // __no_operation();                       // For debug
    while (1)
    {
        P6OUT ^= BIT6;         // Toggle LED
    }
}

void clock_setup()
{
    // Setting clock to 24Mhz
    P2SEL1 |= BIT6 | BIT7;          // P2.6~P2.7: crystal pins

    FRCTL0 = FRCTLPW | NWAITS_2;    // FRAM: 2 wait states

    do
    {
        CSCTL7 &= ~(XT1OFFG | DCOFFG);  // Clear XT1 and DCO fault flag
        SFRIFG1 &= ~OFIFG;
    }
    while (SFRIFG1 & OFIFG);        // Test oscillator fault flag

    __bis_SR_register(SCG0);        // disable FLL
    CSCTL3 |= SELREF__XT1CLK;       // Set XT1 as FLL reference source
    CSCTL0 = 0;                     // clear DCO and MOD registers
    CSCTL1 = DCORSEL_7;             // Set DCO = 24MHz
    CSCTL2 = FLLD_0 + 731;          // DCOCLKDIV = 24MHz
    __delay_cycles(3);
    __bic_SR_register(SCG0);        // enable FLL

    while (CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1))
        ; // wait till FLL locked

    CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK; // set XT1 (~32768Hz) as ACLK source
    // default DCOCLKDIV as MCLK and SMCLK source
}

**Attention** This is a public forum