"MSP430: Trouble Writing Memory Block at 0xf800 on Page 0 of Length 0x56: No error
Cannot write to target"
While trying to program a TSSOP MSP430 on a PCB, I get an error that says "Load program Error." in CCSv5
I have an MSP430 on a PCB which breaks out the 4 J-Tag pins. (VCC, Test, Reset, and Ground).
The PCB design enables it to be isolated from the rest of the circuit while programming as well.
This is the exact chip as what comes with the launchpad in a different packaging. I can program on the DIP package just fine, so I know it's possible to download the code.
Any ideas?
Thanks