I recently started using the Launchpad with CCSv5.2 However, when I attempt to enter a debug state I get an error saying "Error connecting to the target: Unknown device" or " Error Initializing emulator: Could not find MSP-FET430UIF on specified Com Port.".....as many others have, judging by the number of posts on this issue.
It appears that there is a USB driver conflict between my MSP-FET430UIF and the Launchpad USB driver. If I uninstall the MSP-FET430UIF USB driver and restart my PC, the Launchpad works fine. However with the MSP-FET430UIF USB drivers installed, trying to launch a Launchpad debug sessions always results in one of the two error messages above.
I would be interested in hearing from a TI EMPLOYEE on a confirmation of this issue.