Hi everybody,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everybody,
Marco2002 said:But I find being really very very strange that I’ve not been able to solder an SMD device with a reflow oven, nor with an hot air gun, especially considering that the temperature I’ve used in my last attempts was 225°C
So maybe your problem is not soldering at all. - That's why I suggested to use soldering iron and supposedly have same results. Maybe it's just PCB routing or manufacturing or chip orientation error or something like that, not related to how you solder chip..
Things usually start working when done right :)Marco2002 said:I replaced the 10nF capacitor with a 2.2nF capacitor, and now everything is working as expected.
Instead of using a 2.2nF cap (which makes the timing for the reset lien quite short) a larger one can be used if there is a series resistor between the pullup/capacitor combo and the RST pin. This way, the SBW signals are decoupled from the capacitor by the series resistor (1k should be enough) while the pulldown effect of the capacitor at power-up is maintained.
VCC
|
R
----R----RST/SBW
|
C
|
GND
**Attention** This is a public forum