This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

16-bit IR receiver data through Serial?



Hi All,

Glad to be back with an issue again. Recently i've been trying to receive data from an IR remote which used 38KHz Txer and an Encoder(HOLTEK's HOL6221A). I was able reverse engineer and got the codes beneath the keys(Row and Column) from the encode's datasheet. I'm using TSOP1738 as IR receiver. The data when Txed from Remote to IR Rxer,it is being received perfectly(Checked in Oscilloscope) though there timing constraints to be considered in depth. 

I'm trying to receive and decode the 16-bit data from Remote using MSP430 Launchpad. I tried a for loop with an Interrupt enabled port pin(P1.3) to 16-bit long data.But couldn't find it useful. Then i figured out that it is possible and moved on to serial commn. When i'm trying to Rx data from UART Rx pin, using the below code, i was unsuccessful in doin so. I can't understand the problem with the code at all. I'm trying to watch the data using CCS Serial Window(with Target Config.) but couldn't have gone to Rx ISR at all even though i pressed the remote continuously. Is it the problem with interrupt triggering or the Hardware ,or the method i'm following.?? How can i achieve receiving the data(16-bit). Any other alternatives like SPI and I2C??? How it can be done? 

After receiving the data, how i can check and compare and perform the actions accordingly to the key pressed.??? 

Please look the at Serial Rx module i wrote. The Remote's key configurations are there at first. 

/*
Remote Controller Key Configurations

SW1 - R1,C7 - K25  --  0001 100 0/1
SW2 - R1,C6 - K21  --  0010 100 0/1
SW3 - R2,C7 - K26  --  1001 100 0/1
SW4 - R2,C6 - K22  --  1010 100 0/1
SW5 - R3,C7 - K27  --  0101 100 0/1
SW6 - R3,C6 - K23  --  0110 100 0/1
SW7 - R1,C8 - K29  --  0011 100 0/1
SW8 - R2,C8 - K30  --  1011 100 0/1
SW9 - R3,C8 - K31  --  0111 100 0/1

*/

#include "msp430g2553.h"
//#define TXLED BIT0
#define RXLED BIT0
#define RXD BIT1


static unsigned char IR_data[16];
int i = 0;

void main (void)
{
	WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT

	   DCOCTL = 0; // Select lowest DCOx and MODx settings<
	   BCSCTL1 = CALBC1_1MHZ; // Set DCO
	   DCOCTL = CALDCO_1MHZ;

	  P2DIR = 0xFF; // All P2.x outputs<         //Disabling PORT2
	  P2OUT &= 0x00; // All P2.x reset

	  P1DIR |= RXLED;                    
	  P1SEL |= RXLED;                     
	  P1SEL |= RXD ;
	  P1DIR |= RXD;
	

	     UCA0CTL1 |= UCSSEL_2; // SMCLK
	     UCA0BR0 = 0x08; // 1MHz 115200
	     //UCA0BR1 = 0x00; // 1MHz 115200
	     UCA0MCTL = UCBRS2 + UCBRS0; // Modulation UCBRSx = 5
	     UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
	     UC0IE |= UCA0RXIE; // Enable USCI_A0 RX interrupt

	    
	     	__bis_SR_register(CPUOFF + GIE); // Enter LPM0 w/ int until Byte RXed
	     	   while (1)
	     	   { }

 }

#pragma vector=USCIAB0RX_VECTOR __interrupt void USCI0RX_ISR(void) { P1OUT |= RXLED; //for (i = 0; i <= 16; i++) IR_data[i++] = UCA0RXBUF; // RX next character if (i == sizeof IR_data - 1) // RX over? UC0IE &= ~UCA0RXIE; // Disable USCI_A0 RX interrupt P1OUT &= ~RXLED; }

  • did u try different baud rates. Try 9600 baud rate.

  • Hi Mr.Sri,

    Thank you for the response. Yeah, I've tried with 9600 it is working(with some config settings it is working with other Bauds too).

    But can 16-bit data be Rxed? I can't view what exactly is coming through COM in Serial Terminal of CCS. How can we compare and do perform actions accordingly and how it (Buf) can be cleared after checking and action? 

    Thanks n  Regards,

    Venkat

  • I think you are on the wrong track.

    The IR remote control probably has a CPU cycle that varies with temperature and battery condition. Thus the IR signal it transmits does not have precise timing either. If you use a UART to receive the "bits", the result is not reliable.

    There are lots of people use lots of different uC to do it. Find them on the internet. The specific uC they use do not matter. The specific code they wrote does not matter either. It is the principle behind the code that you have to lean.

    -- OCY

  • Hi OCY,

    Thank you very much for the suggestion.Surely  I'll dig into that. So you're saying that it is not possible to decode,detect n check&Validate the data from IR Remote using MSP430??? Or the method like UART is not reliable? How can we able to sense it then? Would you suggest one which can use MSP430???

    Thanks& Regards,

    Venkat

  • VenkataSainath Ravikanti said:
    Or the method like UART is not reliable?

    More this one. UART is asynchronous. It means bot sides assume a certain baudrate. If the assumptions do not match, communication is impossible.

    I suggest using a timer capture input to record the exact timing of the incoming signals, then analyze them once received (by calculating the average, min, max or such). This will auto-adjust to any transmitter baudrate (within limits, off course)

**Attention** This is a public forum